Flash remapping in imxrt1064

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash remapping in imxrt1064

Jump to solution
1,065 Views
karthik1
Contributor I

Hi sir,

1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?

2) Is it XIP mode is supported in internal flash on imxrt1064?

 

thanks and regards 

Karthik N E

0 Kudos
Reply
1 Solution
996 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Karthik N E, 

1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?

Yes, it is possible to remap the on-chip flash 

2) Is it XIP mode is supported in internal flash on imxrt1064?

Yes, XIP is supported in the on-chip flash of the RT1064


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
997 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Karthik N E, 

1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?

Yes, it is possible to remap the on-chip flash 

2) Is it XIP mode is supported in internal flash on imxrt1064?

Yes, XIP is supported in the on-chip flash of the RT1064


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply