Flash remapping in imxrt1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Flash remapping in imxrt1064

跳至解决方案
1,132 次查看
karthik1
Contributor I

Hi sir,

1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?

2) Is it XIP mode is supported in internal flash on imxrt1064?

 

thanks and regards 

Karthik N E

0 项奖励
回复
1 解答
1,063 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Karthik N E, 

1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?

Yes, it is possible to remap the on-chip flash 

2) Is it XIP mode is supported in internal flash on imxrt1064?

Yes, XIP is supported in the on-chip flash of the RT1064


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,064 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Karthik N E, 

1)Is it possible to remap the internal flash(4MB) address using flash remapping method in imxrt1064?

Yes, it is possible to remap the on-chip flash 

2) Is it XIP mode is supported in internal flash on imxrt1064?

Yes, XIP is supported in the on-chip flash of the RT1064


Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复