Hi All
I also note that the i.MX RT FlexRAM applicationAN12077 note requires updating to include the i.MX RT 117X. However by experimenting with its operation it was possible to work out details of its default setting (when no eFUSES have been blown).

As illustrated in this diagram the default is for no OCR to be enabled, 256k DTC and 256k ITC.
The individual banks are configured with the first 4 assigned to DTC, the second 4 to ITC, the next 4 to DTC and the final 4 to ITC again.
The actual run-time reconfiguration is otherwise compatible with the i.MX RT 105x and i.MX RT 106x parts.
For more information see the chapter "RAM and Cache" in the uTasker i.MX RT 117X developer's guide at https://www.utasker.com/docs/iMX/i.MX_RT_1170_uTasker.pdf
Regards
Mark
[uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training, solutions to problems or rapid product development requirements
For professionals searching for faster, problem-free Kinetis and i.MX RT 10xx developments the uTasker project holds the key: https://www.utasker.com/iMX/RT1064.html