FLEXCAN-TransferReceiveNonBlocking quickly fails sending data in the CAN bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FLEXCAN-TransferReceiveNonBlocking quickly fails sending data in the CAN bus

2,717 次查看
rithic
Contributor II

Hello community,

I am using i.MXRT1176 processor and I am using MATLAB 2021b with NXP MBDT version 1.3 for RT MCU. I am working with the CAN bus in transfer mode. I am having a callback function that works perfectly fine until I send a packet in the CAN using a PCAN. When I send the CAN message the CAN bus freezes and in the CAN bus I see an OVERRUN status. I have attached the code and the image of the PCAN window as well

0 项奖励
回复
3 回复数

2,669 次查看
mayliu1
NXP Employee
NXP Employee

Hi @rithic ,

Thank you so much for your interest in our products and for using our community.

From your PCAN window, we can see PCAN just send 1 CAN frame data to MIMXRT1176-EVKB board, then MIMXRT1176 project got OVERRUN status.

mayliu1_0-1732522206268.png

1: I suggest you check whether your  flexcan_callback  function responds and processes the received CAN frame data promptly and efficiently. I think it is very important.

2:I also suggest you to check whether there are other tasks or interrupts in your project that are consuming a large of CPU time, It  may prevent the CAN receive interrupt from responding promptly.  Please try to optimize the processing time.

3: I think you can do validation on your side, set MIMXRT1176 project only receive CAN frame data , do not send CAN frame data, then check whether the project still got overrun error. 

 

Wish it helps you.
If you still have question about it, please kindly let me know.

 

Best Regards

mayliu

0 项奖励
回复

2,573 次查看
rithic
Contributor II

Hi @mayliu1 


Thanks for your message. The Issue I identified was with the timing configured in the BUS. Now its working fine without any issues

0 项奖励
回复

2,545 次查看
mayliu1
NXP Employee
NXP Employee

Hi @rithic ,

Thanks for your update information.

I'm very happy that your problem is solved.

If you have any new issues, welcome to create new case.

I  will close this case, Thanks for  your interest in the NXP MIMXRT product.

Wish you a nice day!

 

BR

mayliu

0 项奖励
回复