External Memory Controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External Memory Controller

1,550 次查看
13692631114
Contributor I

The speed at which EMC connects to SDRAM is different from the description in the RT1020 reference manual and user manual. Which one is correct?

0 项奖励
回复
1 回复

1,542 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi,

RT1020 SEMC module can run at 166MHz, so the SDRAM should be able to run at 166MHz. But the IO has overshoot problem. It will have EMI/EMC problem if hardware design is not very perfect. It is strongly recommended to follow the hardware development guide. 

 

Regards,

Jing

0 项奖励
回复