Debugging and tracing the RT1060 EVK using IAR and I-Jet probe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging and tracing the RT1060 EVK using IAR and I-Jet probe

1,088件の閲覧回数
shai_b
Senior Contributor II

Hello Team,

My customer is trying to use Trace while debugging our RT1060 EVK.

The i.MXRT1062 that is used on the i.MXRT1060 eval board is capable of SWO but when looking at the schematic of the board it seems that GPIO_B0_13 that is listed as “ARM_TRACE_SWO” is used for the LCDIF:

shai_b_0-1603457425925.jpeg

Could you please advise if there be something to be done in order to make the SWO pins can support Tracing on the eval-board using #IAR #I-Jet debugger?

Thanks in advance 

Regards,

Shai 

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,076件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Shai,

I recommend you to use the JTAG_TDO pin for SWO that is already routed to the debug header.

image.png

image.png

Please check the link below that explains how you can use SWO feature for MIMXRT1064 board but it can work as well for your board.

SWO with NXP i.MX RT1064-EVK Board - NXP Community

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored. Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 件の賞賛
返信