Debug encrypted HAB image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug encrypted HAB image

Jump to solution
2,162 Views
dh1
Contributor II

Hello

We are using HAB with an encrypted image and download the image with the MfgTool.
The application runs this way, but we need to debug a problem.

The problem only happens with the encrypted image (not with the same code and an unencrypted image), therefore we need to debug the encryped image.

Is it possible at all to debug an encrypted image with the SWD debugger?

Thanks and regards,
Daniel

Tags (1)
0 Kudos
Reply
1 Solution
2,155 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is it possible at all to debug an encrypted image with the SWD debugger?
-- No, I'm afraid not.
I'd like to suggest you to consider other debug trick like terminal print, etc.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,156 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)Is it possible at all to debug an encrypted image with the SWD debugger?
-- No, I'm afraid not.
I'd like to suggest you to consider other debug trick like terminal print, etc.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply