Confusion regarding Minimum OCRAM Size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Confusion regarding Minimum OCRAM Size

ソリューションへジャンプ
3,750件の閲覧回数
gh78731
Contributor III

Regarding AN12077 : Using the i.MX RT FlexRAM (Rev 3, 01/2021)
https://www.nxp.com/docs/en/application-note/AN12077.pdf

and

i.MX RT Knowledge Base : Reallocating the FlexRAM
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Reallocating-the-FlexRAM/ta-p/1117649

 

AN12077 on page 4, says "The minimum configuration of OCRAM is 64 KB (see Table 1)."

Then it proceeds to offer configurations 1, 3, 4 and 6 that violate this rule, with only 32 kB.

Does this mean that configurations 1,3, 4, and 6 should not be used, and should probably be grayed out, or removed from the table?


Then in the Knowledgebase article "Reallocating the FlexRAM", on approximately lines 17 and 18, says
"One thing that's important to mention is that the ROM in all the RT10xx parts uses 32KB of OCRAM, hence you should keep at least 32KB of OCRAM when reallocating the FlexRAM..."

This would suggest that all entries in table 1 in AN12077 are valid, and the Note under section 2.1.1.1 is in error.

Which one is correct?

I would like a clarification before I start reallocating SRAM, because the allocation using the eFuses is permanent, and can not be reversed.

Thanks,
--- Graham

ラベル(4)
タグ(2)
0 件の賞賛
返信
1 解決策
3,723件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Graham, 

Thanks for catching this! I already fixed the community document. Regarding the amount of OCRAM, please be aware of the following part of the note. 

victorjimenez_0-1620927201234.png

For the RT1010, the amount of OCRAM needed is 32KB. For all the other RT10xx families, you need 64KB. 

Regards,
Victor 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,733件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Graham, 

I'm checking this internally, I will give you an update as soon as possible. Thanks for your patience.

Regards,
Victor 

0 件の賞賛
返信
3,724件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Graham, 

Thanks for catching this! I already fixed the community document. Regarding the amount of OCRAM, please be aware of the following part of the note. 

victorjimenez_0-1620927201234.png

For the RT1010, the amount of OCRAM needed is 32KB. For all the other RT10xx families, you need 64KB. 

Regards,
Victor 

0 件の賞賛
返信
3,717件の閲覧回数
gh78731
Contributor III

Victor:

OK, that clarifies things.

Thanks for getting the documents fixed.

--- Graham

 

==