Code generation Matlab

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code generation Matlab

1,469 Views
erikraynolds
Contributor IV

Is there any example that clearly demonstrates Code-Generation (Matlab Coder, Embedded Coder) for RT-device -with Cortex-M7 CPU?

Picture1.png

Tags (1)
0 Kudos
Reply
1 Reply

1,446 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is there any example that clearly demonstrates Code-Generation (Matlab Coder, Embedded Coder) for RT-device -with Cortex-M7 CPU?
-- As I know, until now, NXP hasn't provided any application notes or similar documents which demonstrate Code-Generation (Matlab Coder, Embedded Coder) for RT-device -with Cortex-M7 CPU.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply