Can I.MX RT1050 XIP from encrypted parallel nor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I.MX RT1050 XIP from encrypted parallel nor?

ソリューションへジャンプ
2,008件の閲覧回数
loverdeg
Contributor II

Can I.MX RT1050 XIP from encrypted parallel nor?

I'm assuming not considering I see no mention of it in any documentation.

Also what sort of performance bottle-neck would be seen with XIP from parallel flash? (encrypted or not)

How does this bottleneck compare to XIP from ultraflash or qpsi flash?

ラベル(1)
1 解決策
1,772件の閲覧回数
343mjt
Contributor II

Hi Artur,

What other options are there for encrypted XiP support through means other than FlexSPI/serial NOR flash?

Thanks

Matt

元の投稿で解決策を見る

3 返答(返信)
1,772件の閲覧回数
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 件の賞賛
返信
1,772件の閲覧回数
art
NXP Employee
NXP Employee

No, there is no encrypted XiP support for parallel NOR Flash. The encrypted XiP is only supported for serial NOR Flash via the FlexSPI interface.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,773件の閲覧回数
343mjt
Contributor II

Hi Artur,

What other options are there for encrypted XiP support through means other than FlexSPI/serial NOR flash?

Thanks

Matt