IMXRT1064 LVDS CLK input usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1064 LVDS CLK input usage

809 Views
dbasilio83
Contributor II
Hello
Our query relates to the LVDS 'CCM_CLK1_P/CCM_CLK1_N' external clock input on the IMXRT1064. It states in the datasheet:
"One general purpose differential high speed clock Input/output (LVDS I/O) is provided. It can be used:
• To feed external reference clock to the PLLs and further to the modules inside SoC."
We would like to run the timer modules (GPT, TMR) on the IMXRT1064 off this external 100MHz LVDS clock, but run the ARM core clock off 600MHz that is generated from the external 24MHz crystal.
 
Our question is:
  1. Can one run the ARM core clock (AHB_CLK) unsynchronized from the peripheral bus clock (IPG_CLK) ? 
Thank you in advance
Labels (1)
0 Kudos
Reply
1 Reply

751 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Daniel,

Please check my reply on this thread.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply