Can I.MX RT1050 XIP from encrypted parallel nor?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can I.MX RT1050 XIP from encrypted parallel nor?

跳至解决方案
1,962 次查看
loverdeg
Contributor II

Can I.MX RT1050 XIP from encrypted parallel nor?

I'm assuming not considering I see no mention of it in any documentation.

Also what sort of performance bottle-neck would be seen with XIP from parallel flash? (encrypted or not)

How does this bottleneck compare to XIP from ultraflash or qpsi flash?

标签 (1)
1 解答
1,726 次查看
343mjt
Contributor II

Hi Artur,

What other options are there for encrypted XiP support through means other than FlexSPI/serial NOR flash?

Thanks

Matt

在原帖中查看解决方案

3 回复数
1,726 次查看
jay_heng
NXP Employee
NXP Employee

You can also try this tool, with this tool, You can flash bare image into various boot devices easily and don't need to care about headers (ivt, boot data...)

GitHub - JayHeng/nxp-sec-boot-ui: A one-stop GUI tool to work with NXP MCU (Kinetis, i.MXRT, LPC) RO... 

0 项奖励
回复
1,726 次查看
art
NXP Employee
NXP Employee

No, there is no encrypted XiP support for parallel NOR Flash. The encrypted XiP is only supported for serial NOR Flash via the FlexSPI interface.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,727 次查看
343mjt
Contributor II

Hi Artur,

What other options are there for encrypted XiP support through means other than FlexSPI/serial NOR flash?

Thanks

Matt