CBATTError Writing is not enabled for Alexa MCU on iOS devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CBATTError Writing is not enabled for Alexa MCU on iOS devices

2,563 Views
anon-aacc420858
Contributor I

I am trying to provision the Alexa MCU peripheral with the WiFi credentials so it's able to connect to a WiFi network automatically. I've tried the app that is currently live in the App Store (version 1.4.8) but crashes when I try to start the BLE provision.

I've also used the Swift sample code (version 1.4.3) with no result and there are some issues when it crashes as it's trying to force unwrap an optional with a nil value inside. 

This is replicable using the provided Swift code sample (version 1.4.3) when trying to write the JSON value to the MCU.

I have successfully connected an iPhone to the MCU via Bluetooth and when I am writing the value I get the next error.

Error Domain=CBATTErrorDomain Code=3 "Writing is not permitted." UserInfo={NSLocalizedDescription=Writing is not permitted.}

The discovered CBCharacteristicProperties are the mask of the read (2) and write (8) properties so the discovered properties in the debugging console are shown as:

po service.characteristics!.uuid

    3E9D2532-2F00-11E9-9602-A44CC81C989A

po service.characteristics!.properties

    ▿ CBCharacteristicProperties - rawValue : 10

I should be able to write anything into the device as I have received the correct permissions. Whenever I try to do this in the didDiscoverCharacteristicsFor delegate method I get the previous CBATTError not letting me write anything to the device.

Captura de pantalla 2020-03-26 a las 17.42.43.png

However, I am able to read values from the MCU and the problem only shows when writing the value.

Just in case I have tried another app like LightBlue to write a sample value and connecting to the MCU in the console using the screen command to see if any error comes up but nothing shows up. 

The tests have been done on the MCU running version 1.0.10 Apptype: AppA and on two iPhones: X (iOS 13.4) and 6S (iOS 13.3.1) and in both cases the same error prevents writing. 

The Android app is working correctly and writes the JSON to the device without a problem. This has to be an iOS error I am not seeing with CoreBluetooth.

Tags (3)
0 Kudos
Reply
2 Replies

2,383 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Javier,

Hope you are doing well.

Could you please try provisioning with WIFI. Please follow the steps to section 4 in the getting started. 

SLN-ALEXA-IOT: Getting Started with Alexa Voice Service | NXP 

Let me know if you are having any issues with the provisioning using WIFI.

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply

2,383 Views
anon-aacc420858
Contributor I

Is it not possible to provision the WiFi credentials via Bluetooth on iOS devices? This is just to discard that part of the code and only do it with WiFi.

0 Kudos
Reply