Bulk transfer for USB host camera interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bulk transfer for USB host camera interface

1,901 Views
pjanco
Contributor III

Hi,
I am trying to connect a face recognition camera to USB host interface on EVK1060 board and it is not functional with SDK example "host_video_camera_freertos". By debugging the code I figure out that a camera support only "bulk" transfer type and SDK example have implemented only "isochronous" transfer type.

Can you provide an example or any useful information for bulk camera host?

Regards, Peter.

 

 

0 Kudos
Reply
1 Reply

1,890 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Peter,

The USB examples on the i.MXRT1060 are a bit limited and offered as proof of concept. USB video/audio can get a bit tricky, there are some threads on this topic on the communities but most are focused on USB audio rather than USB video, and there is not a definitive document or example for reference.

My apologies for the inconvenience.

Regards,
Gustavo

0 Kudos
Reply