Binary image flashing process for i.MX RT600EVK's cores

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Binary image flashing process for i.MX RT600EVK's cores

跳至解决方案
1,385 次查看
subhash_ponnusamy
Contributor II

Hi,

I'm using MIMXRT600 EVK for my current project.

There are 2 cores in this EVK. Core 1 is cortex M33 and second one is cadence tensilica HiFi4 DSP processor.

I need to use both cores for my project.

DSP core for audio processing and cortex M33 core for general purposes.

Do I need to flash two separate binary image for the cores or a single binary image is sufficient to operate both cores.

标记 (2)
0 项奖励
回复
1 解答
1,375 次查看
jason_tseng
NXP Employee
NXP Employee

Hello,

You don't need to flash it twice.

By default two images will be combines together then generated to one axf or binary file for flashing.

Thanks

在原帖中查看解决方案

1 回复
1,376 次查看
jason_tseng
NXP Employee
NXP Employee

Hello,

You don't need to flash it twice.

By default two images will be combines together then generated to one axf or binary file for flashing.

Thanks