Binary image flashing process for i.MX RT600EVK's cores

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Binary image flashing process for i.MX RT600EVK's cores

ソリューションへジャンプ
1,384件の閲覧回数
subhash_ponnusamy
Contributor II

Hi,

I'm using MIMXRT600 EVK for my current project.

There are 2 cores in this EVK. Core 1 is cortex M33 and second one is cadence tensilica HiFi4 DSP processor.

I need to use both cores for my project.

DSP core for audio processing and cortex M33 core for general purposes.

Do I need to flash two separate binary image for the cores or a single binary image is sufficient to operate both cores.

タグ(2)
0 件の賞賛
返信
1 解決策
1,374件の閲覧回数
jason_tseng
NXP Employee
NXP Employee

Hello,

You don't need to flash it twice.

By default two images will be combines together then generated to one axf or binary file for flashing.

Thanks

元の投稿で解決策を見る

1 返信
1,375件の閲覧回数
jason_tseng
NXP Employee
NXP Employee

Hello,

You don't need to flash it twice.

By default two images will be combines together then generated to one axf or binary file for flashing.

Thanks