Addr Pin allocation between RT1052 and SDRAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Addr Pin allocation between RT1052 and SDRAM

2,378 Views
1509831698
Contributor I

We need to add one SDRAM in our project on IMX RT1052,here comes a question since this is my first time to use SDRAM and I can't find the official explantion both on NXP and the SDRAM manufactor.The RT1052 has 13bit pin(A0-A12) address  to allocate while the SDRAM we select just have 12bit pin (SA0--SA11), how should I connect them togerther. PS.The SDRAM we select is W9812G6JB from WinBond.

Labels (1)
0 Kudos
Reply
2 Replies

2,228 Views
carstengroen
Senior Contributor II

Have a look at the schematics for the EVK for the RT1052: https://www.nxp.com/webapp/Download?colCode=MIMXRT1050-EVK-DESIGNFILES-A1&appType=license 

(more here: i.MX RT1050 Evaluation Kit|NXP )

(just a note, I would personally not select a SDRAM that has a datasheet that dates back to 2012. In my RT1062/1064 designs I use the same SDRAM as NXP uses on their EVK's, make things easier. But maybe you have good reasons to use the Winbond device)

Below is a snip of the schematic from one of my designs, its for RT1062/RT1064 but If I'm not mistaken, the 1052 is very similar, but please check carefully !?!

pastedImage_1.png   pastedImage_2.png

0 Kudos
Reply

2,228 Views
1509831698
Contributor I

Ths. The EVK default use 256M SDRAM,so it need 13bit address pin and we just need 128M SDRAM considering cost and our application.While the common  numbers of address pin in 128M SDRAM I have found are all 12bit with A0--A11 for row and A0-A8 for column.That's the confuse I have meet.

0 Kudos
Reply