Additional SDRAM input using CS1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Additional SDRAM input using CS1

2,044 次查看
youngsangcho
Contributor I

Hi,

I'm trying to use an additional SDRAM(total 2 SDRAM) to RT1064.

It is connected  CS0(GPIO_EMC_29) to the first SDRAM as EVK board and I'm going to use  SEMC_CSX0(GPIO_EMC_41) for CS1 of the second SDRAM.

However, an error occurs in the MUX_CSX0 PIN as shown below.

youngsangcho_0-1613163165643.pngyoungsangcho_0-1613163165643.png

Is it an MCUXpresso Config tool bug or I can't use the SEMC_CSX0(GPIO_EMC_41)  pin for SDRAM CS1?

Thank you,

YC

 

 

标签 (1)
标记 (2)
0 项奖励
回复
2 回复数

2,006 次查看
youngsangcho
Contributor I

Thanks for the confirmation.

Young 

2,012 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  It is possible to use SEMC_CSX0(GPIO_EMC_41) as CS1 for the second SDRAM.
Customers can use i.MX Pins tool.

https://www.nxp.com/design/designs/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX

 

Regards,
Yuri.

0 项奖励
回复