AD SAMPLE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AD SAMPLE

3,978 Views
bisheng
Contributor I

我的问题如下:

用MIMXRT1011 51号管脚   GPIO_AD_07通道采集电池电压,电池电压7.3V ,经75K、39K电阻分压后给MCU采集,理论应该为2.50V,实测2.61V,采样数值不准确,请问MCU的IO口配置是否有影响?该怎么配置,thank you !

 

得到的回复如下:

你好,

我们发现ADC采样结果会受到异步ADC时钟供电源的干扰,造成采样结果产生大范围偏差。

我们建议客户使用IPG时钟,并且将ADCx_GC[ADACKEN] 位设置成 0;

如果需要使用ADC异步时钟,则需要IPG时钟设置为无效。

希望对你的问题有所帮助

 

 

 

时间过去很久了  AD这一问题还没解决  软件上不知道怎么配置 看能否发些AD例程过来  帮我解决这个问题 谢谢  我们是做打印机的

Labels (1)
0 Kudos
Reply
3 Replies

3,966 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
非常感谢使用NXP产品,很高兴为你提供技术支持!
关于软件实现,就是在ADC初始化过程中,在ADCx_CFG寄存器中设置ADICLK选择IPG clock作为时钟源,接着ADCx_GC[ADACKEN] 位设置成 0,其他软件部分保持不变。
至于ADC例程,我建议参考SDK软件库中的ADC例程,可以在其例程基础上很容易修改ADC配置选项。
同时,我建议你从多方面查找问题,比如VDDADC是否稳定,采样脚附件是否有高频信号等。
希望这些建议对你能有所帮助。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,962 Views
bisheng
Contributor I

能否提供一下修改好的ADC例程  我这边软件还不会 谢谢!

0 Kudos
Reply

3,955 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
感谢回复,正如我上面说的,你可以通过以下连接下载对应i.MX RT的SDK 软件包,里面就有ADC例程。
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply