9-bit uart MDB protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9-bit uart MDB protocol

1,384 Views
BvLeeuwen
Contributor I

We currently have a system which is controlling an MDB bus and we are investigating if we can move to NXP chips. Everything is looking great, the only thing I can't seem to find is whether 9bit uart works "out of the box". I've read [link], [link] and [link] but these concern the imx6 series and I am still not 100% sure whether it will work on i.MXRT102x without having to bit bang anything.

Does the NXP chip support 9bit uart on hardware level?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Reply

1,375 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

The LPUART of the RT1020 family has the following feature: programmable 7-bit, 8-bit, 9-bit, or 10-bit character length. For more information regarding this, refer to section 44.3.6.1 of the RT1020 reference manual. 

Regards,
Victor 

0 Kudos
Reply