i.MX RT Crossover MCUs Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX RT Crossover MCUs Knowledge Base

Discussions

Sort by:
The i.MX RT700 microcontroller family includes an eIQ Neutron N3-64 NPU for accelerating neural network models. The i.MX RT700 EVK can be combined with a camera and LCD screen to showcase running TinyML vision models on a microcontroller. It's recommended to also go through the basic i.MX RT700 NPU Lab to learn more about eIQ enablement on RT700. The rest of this post will cover using vision models with camera+LCD on i.MX RT700.    i.MX RT700 Camera Hardware Setup: The following hardware is used: i.MX RT700 EVK RK055HDMIPI4MA0 LCD panel Camera Options: USB Camera with USB A to micro-B converter OV7670 parallel camera (with optional wide-angle lens) The USB camera should be attached to the i.MX RT700 EVK on USB OTG port J40. The parallel camera interface is available on J53 and uses FlexIO with eDMA to read in the camera data. AN14836 describes the details. Note that the links in that app note for the demo software do not work but the demo code is in the process of being posted on NXP’s Application Code Hub.  When inserting the parallel camera align it to the left most side, as shown in the image below:       Directions for attaching the LCD panel to the J52 connector on the underside of the i.MX RT700 EVK can be found on this Community post.  Note that there are multiple names used for the LCD panel and all these part numbers refer to the exact same panel: RK055HDMIPI4MA0 RK055MHD091 RK055MHD091-CTG RK055MHD091A0-CTG i.MX RT700 Vision ML Examples: There are two vision AI/ML examples for i.MX RT700 available today: Object Detection (part of AN14718) Hand Gesture Recognition Both of these examples use a USB camera.  i.MX RT700 Vision MPP Examples:  The Media Processing Pipeline (MPP) interference examples in i.MX RT700 MCUXpresso SDK 26.06 and later support both parallel and USB camera interfaces. These SDK examples are only available for command line GCC and VS Code MCUXpresso SDK layouts. They are not available for MCUXpresso IDE, IAR, or Keil.    A parallel camera is used by default in the RT700 MPP projects. A USB camera can be enabled by adding a USE_USB_CAMERA declaration in the project's CMakeLists.txt file by adding the following macro:   mcux_add_macro(     CC "-DUSE_USB_CAMERA"     CX "-DUSE_USB_CAMERA" ) However it's important to note that the camera_usb_final_fr_app_view project is setup to use USB camera by default, but it only works with a very specific HM2131 camera. All other MPP demos can work with most generic USB cameras.   
View full article
​​迁移重点​​: ​​检查GPIO配置​​:利用新时序建议优化设计。 ​​更新SDK至25.06+​​:确保芯片版本识别和ROM API兼容。 ​​验证SEMC设计​​:若使用CSX1/2/3,需按ERR052401调整时序。 ​​工具链升级​​:J-Link v8.38+和MCUXpresso脚本更新。   0. 本文目的    若您并未遇到RT1170 FSGPIO漂移老化问题,请忽略本文档。 若您遇到RT1170A的ERR052351(输出电压>1.98V时参数漂移)和ERR050643(上电瞬间误触发上拉脉冲)问题,并想通过迁移到新硅片RT1170B,请查看本文完成迁移。 ​ 1. 硅片变更 (Silicon Changes)​ ​ ​​GPIO修复​​: 解决了RT1170A的ERR052351(输出电压>1.98V时参数漂移)和ERR050643(上电瞬间误触发上拉脉冲)问题。 影响范围:GPIO_AD/GPIO_LPSR/GPIO_DISP_B2 bank。 ​​ROM更新​​: 清理ROM补丁(不影响开放API)。 ​​HAB API向量表地址​​:从 0x0021_1C0C (A版)改为 0x0021_1C14 (B版)。 ROM_FLEXSPI_NorFlash_ClearCache() 入口地址变更(详见第6节)。 ​​芯片ID变更​​: MISC_DIFPROG 寄存器的 CHIPID 复位值变化: A版: 0x001170A0 B版: 0x001170B0 (需通过bit[7:4]区分:A版= 1011 ,B版= 1100 )。 ​​2. 数据手册变更 (Data Sheet Changes)​ ​ ​​型号命名​​:所有型号后缀从 A 改为 B (例: MIMXRT117xxxxxB )。 ​​GPIO电气规范​​: ​​表37​​:GPIO_AD/LPSR/DISP_B2的驱动电流调整(如DSE=1时IOH从-10mA→-9mA)。 ​​表40​​: 新增 Vpead 参数。 上升/下降时间调整(如DSE=0/SRE=1时从6ns→7.5ns)。 ​​关键建议​​: 3.3V模式:≥25MHz用连续范围模式(Continuous Range),<25MHz用高范围模式(High Range)。 1.8V模式:推荐低范围模式(Low Range)。 ​​其他更新​​: 存储温度范围:-40℃ → ​​-55℃​​。 SDR50/SDR104时序:输入建立时间从2.5ns→2.0ns。 FlexSPI时序:TDVO最大值从4→1,TDHO最小值从2→0。 ​​3. 参考手册变更 (Reference Manual Changes)​ ​ ​​芯片ID识别​​: MISC_DIFPROG[7:4] 复位值从固定值改为​​芯片版本标识​​(A版= 1011 ,B版= 1100 )。 ​​4. 勘误变更 (Errata Changes)​   参考资料:i.MX RT1170A Errata,  i.MX RT1170B Errata​ ​​修复问题​​: 移除ERR052351(GPIO参数漂移)和ERR050643(上电脉冲问题)。 ​​新增问题​​: ​​ERR052401​​:SEMC_CSX1/2/3信号时序退化(SYNC模式最大延迟增加2.4ns)。 ​​规避方案​​: SYNC模式:优先使用SEMC_CSX0或SEMC_RDY作为片选。 Async模式:调整SEMC配置寄存器(SRAMCR1/NORCR1的CES位)。 ​​5. SDK代码变更 (SDK Code Changes)​ ​ ​​SDK 25.06​​(2025年6月底发布)支持B版。 ​​关键代码调整​​: ChipID 和  ROM_API bootloader入口地址  变更 /*! * @brief ROM API init. */ void ROM_API_Init(void) { if (ANADIG_MISC->MISC_DIFPROG == 0x001170a0U) // A版 { g_bootloaderTree = ((bootloader_api_entry_t *)*(uint32_t *)0x0020001cU); } else // B版 { g_bootloaderTree = ((bootloader_api_entry_t *)*(uint32_t *)0x0021001cU); } } FlexSPI缓存清除函数入口地址变更 :ROM_FLEXSPI_NorFlash_ClearCache /*! @brief Software reset for the FLEXSPI logic. */ void ROM_FLEXSPI_NorFlash_ClearCache(uint32_t instance) { uint32_t clearCacheFunctionAddress; if (ANADIG_MISC->MISC_DIFPROG == 0x001170a0U) { clearCacheFunctionAddress = 0x0020426bU; } else if (ANADIG_MISC->MISC_DIFPROG == 0x001170b0U) { clearCacheFunctionAddress = 0x0021a3b7U; } else { clearCacheFunctionAddress = 0x0021a3bfU; } HAB API vector table addresses变更 :从0x0021_1C0C(i.MX RT1170A) to 0x0021_1C14(i.MX RT1170B). SDK无影响,SBL github已经解决。 ​​6. 工具变更 (Tool Changes)​ ​ ​​J-Link​​:需升级至​​v8.38或更高版本​​。 ​​MCUXpresso​​:v24.12及更早版本需更新 RT1170_reset.scp 脚本中的芯片ID检测逻辑。 ​​7. 通用数据手册更新 (Appendix A)​ ​ ​​电压范围​​: NVCC_GPIO重命名为​​NVCC_AD​​(后续版本将恢复原名)。 NVCC_AD/DISP2/LPSR最大值从1.95V→​​1.98V​​。 ​​GPIO模式定义​​: 统一命名:​​连续范围模式​​(原Normal/Derated)、​​低范围模式​​(原Low)、​​高范围模式​​(原High)。 ​​时序优化​​: LPSPI主模式频率上限从30MHz→​​60MHz​​,建立时间从10ns→3ns。 ​​新增警告​​: GPIO_AD/LPSR/DISP_B2的NVCC不可悬空,否则可能漏电​​500μA/每Bank​​。 ​​8. 其他信息​ ​ ​​文档版权​​:示例代码遵循​​BSD-3-Clause许可证​​。 ​​参考文档​: AN14716 MCUXPresso SDK i.MX RT
View full article
Realize a panoramic video layer with OpenGL
View full article
When design a project, sometimes CCM_CLKO1 needs to output different clocks to meet customer needs. This customer does not need to buy a separate crystal, which can reduce costs。The document describe how to make CCM_CLKO1 output different clock on I.MXRT1050. According to  selection of the clock to be generated on CCM_CLKO1(CLKO1_SEL) and setting the divider of CCM_CLKO1(CLKO1_DIV) in I.MXRT1050reference manual. CCM_CLKO1 can output different clock. If CCM_CLKO1 output different clock via SYS PLL clock. We can get the different clock for the application. CLKO1_DIV 000 001 010 011 100 101 110 111 Freq(MHz) 264 132 88 66 52.8 44 37.714 33 For example we want to get 88Mhz output via SYS PLL clock. We can follow the steps as the below(led_blinky project in SDK 😞       1. PINMUX GPIO_SD_B0_04 as CCM_CLKO1 signal.       IOMUXC_SetPinConfig(       IOMUXC_GPIO_SD_B0_04_CCM_CLKO1,              0x10B0u; 2.Enable CCM_CLKO1 signal. CCM->CCOSR |= CCM_CCOSR_CLKO1_EN_MASK; 3.Set CLKO1_DIV to get 88MHZ the clock for the application. CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO1_DIV_MASK)) | CCM_CCOSR_CLKO1_DIV(2); CCM->CCOSR = (CCM->CCOSR & (~CCM_CCOSR_CLKO1_SEL_MASK)) | CCM_CCOSR_CLKO1_SEL(1); 4 We will get the clock as the below. Note: In principle, it is not recommended to output CLOCK in CCM_CLKO1, if necessary, Please connect an 8-10pf capacitor to GPIO_SD_B0_04, and connect a 22 ohm resistor in series to prevent interference.
View full article
[中文翻译版] 见附件 原文链接: https://community.nxp.com/docs/DOC-340813
View full article
Using a different Flash with the RT1050 In IAR/Keil environment , when you change to other flash(not default flash on EVK board), please refer to below AN to modify the code for it. https://www.nxp.com/docs/en/nxp/application-notes/AN12183.pdf
View full article
There are some items to be aware of when using eIQ projects in VSCode with MCUXpresso SDK 26.03   Debugger hangs when debugging eIQ examples on i.MX RT700 in VSCode There are two work-arounds available: 1) Use a JLink to debug the project instead of the default CMSIS-DAP interface. To do this: Install LinkServer Put a jumper on JP20 on the i.MX RT700 EVK, Update the MCULink firmware to use JLink by running C:\NXP\LinkServer_25.12.83\MCU-LINK_installer\scripts\program_JLINK.cmd Take off the jumper on JP20.    2) Alternatively update the linker file in the eIQ project:  Open the MIMXRT798Sxxxx_cm33_core0_flash.ld linker file in Repository->mcusdk->examples->_boards->mimxrt700evk->eiq_examples->tflm_label_image->cm33_core0->gcc  (use the path based on the eIQ project name that you are trying to use) In that linker file go to line 198 to 203 and replace the .ncache section with the code below:   .npu_ncache (NOLOAD) :   {       KEEP(*(.npu_ncache_data))       KEEP(*(.npu_ncache_data*))   } > m_ncache   ASSERT(. < 0x20580000, "Error: .npu_ncache cannot go beyond SRAM P18")   .ncache (NOLOAD) :   {     *(NonCacheable)     . = ALIGN(4);     __noncachedata_end__ = .;     /* define a global symbol at ncache data end */   } > m_ncache       i.MX RT700 eIQ HiFi4 and HiFi1 projects cannot be imported or compiled in VSCode or command line GCC. In VSCode use the "Repository" import option. To compile the projects you must install Xtensa Xplorer, the RT700 license, and RT700 NewLib DSP Configuration file. Then add the following environmental variables: XCC_DIR=/<Xtensa Install Path>/XtDevTools/install/tools/RI-2023.11-win32/XtensaTools XTENSA_CORE=rt700_hifi4_RI23_11_nlib The project can then be compiled with command-line GCC with: west build -p always --sysbuild examples/eiq_examples/tflm_cifar10_hifi4/cm --toolchain armgcc --config flash_debug -b mimxrt700evk -Dcore_id=cm33_core0 Note that if using HiFi1 projects then XTENSA_CORE should be set to rt700_hifi1_RI23_11_nlib   Also an additional compile option called -mlongcalls needs to be used to avoid issues when adding additional operators the ops list. Inside \mcuxsdk\examples\_boards\mimxrt700evk\eiq_examples\tflm_cifar10_hifi4\hifi4 edit the reconfig.cmake file in the mcux_add_xtensa_configuration options:   mcux_add_xtensa_configuration( CC "-DXOS_CLOCK_FREQ=237500000 -std=c99 -mlongcalls" CX "-stdlib=libc++ \ -mlongcalls \ -std=c++17" ) A warning message comes up in eIQ Neutron SDK 3.1.2 If using eIQ Neutron SDK 3.1.2 then the follow warning will appear on the serial terminal during the model initialization: Unable to save model handle, call neutronModelUnprepare() when done This warning is not relevant for Neutron C devices like RT700 and MCX N and can be ignored as it does not impact inference time or accuracy. It will be fixed in the next eIQ Neutron SDK release. Some eIQ files that are commonly modified are shared among all eIQ examples For example, the Neutron libraries are shared among all eIQ examples. This can cause version compatibility issues with the default eIQ examples if the eIQ Neutron libraries are updated with eIQ Neutron SDK. This is because the eIQ projects in MCUXPresso SDK were converted using Neutron Converter 3.0.0 and the Neutron libraries in the SDK are shared among all eIQ projects.  To work around this, either revert the Neutron libraries back to version 3.0.0 or else download a separate repository to use the default eIQ examples. 
View full article
RT600 ROM API example for w25q128fw support.
View full article
There are two important memory locations used during eIQ inferencing on microcontrollers: modeldata: Location of the model in memory. Can be located in RAM or Flash. Inference time will be faster if it is located in RAM. s_tensorArena: Memory area that is used for input, output, and intermediate arrays. Must be located in RAM. The MCUXpresso SDK eIQ projects create a s_tensorArena buffer that is placed in RAM and used by the model. In the MCUXpresso SDK projects, the default size for this buffer is 256 KB in size and the size is set by the kTensorArenaSize variable, which is declared in the model_data.h header file in the MCUXpresso SDK examples:   The s_tensorArena buffer is declared in the eIQ MCUXpresso SDK projects in the model.cpp file   Size of TensorArena for a model is based on the input, output, and scratch memory of the largest operator in the model:     It is estimated during Neutron Conversion in the last Total Data field. However it’s always slightly smaller than actual amount required.     The actual buffer size used is printed out during inference by using the s_interpreter- >arena_used_bytes(); API call after model initialization. This is automatically done in the MCUXpresso SDK eIQ examples:   Thus the tensorArena buffer size can be optimized in a project for the particular model by running the project at least once and then the kTensorArenaSize variable can be set to the actual used size as it will remain constant for a particular model. Buffer size requirements are model-specific and will depend on the structure and complexity of each model.   The TensorArena size required is often the same regardless of using the original unconverted model or a NPU converted model, but sometimes the NPU reduces the required size. And occasionally the buffer size must be larger for an NPU converted model so it is quite model dependent. Beyond the model inferencing specific memory requirements, there will also be RAM and Flash required for generating the input data for a model (camera, sensor, etc) and any output handling (LCD, notification, etc).  MCX N Specific Memory Details for Neutron NPU: By default the model is placed into the internal flash because in model_data.h it is declared with: static const uint8_t model_data[] __ALIGNED(16) __PLACEMENT = {   By removing the const keyword, then the model will be placed into RAM during runtime and slightly improve the inference time. static uint8_t model_data[] __ALIGNED(16) __PLACEMENT = { As an example, doing this in the CIFAR10 MCUXpresso SDK example improves the inference time from 7.032ms to 5.524ms. Note that the kTensorArena variable must also be reduced from the default 256,000 bytes to 44,848 in order to fit in the internal RAM. The inference time improvement is model specific. However putting the model into RAM could not be done for the Label Image MCUXpresso SDK example because that model is too big and there is not enough RAM available for the model plus the tesnorArena buffer (which must be in internal RAM).  i.MX RT700 Specific Memory Details for Neutron NPU: See the i.MX RT700 eIQ Neutron NPU Enablement and Performance app note (AN14700) for more details about using eIQ Neutron NPU on i.MX RT700.  On i.MX RT700 the NPU has access to 5.5 MB of internal RAM from address 0x2000_0000 to 0x2058_0000 which consists of partitions SRAM P0 to SRAM P17. The model should be located inside this RAM area if it is placed in internal RAM. If using external memory, then the eIQ libraries will automatically copy the necessary model data to that internal memory location (see section below). The s_tensorArena buffer must also be within this 5.5MB RAM memory area. If the tensorArena buffer is located outside this 5.5MB area the model will still run but the inference results will be incorrect.      For i.MX RT700 eIQ projects, by default the model is placed at location 0x2040_0000 in RAM using the modeldata location name. For larger models, the RAM allocated by default in the eIQ SDK example projects for the s_tensorArena buffer or modeldata area may not be sufficient. In such case, the NCACHE_REGION size (where the s_tensorArena buffer is located) and modeldata size can be increased in the SDK project settings by modifying the linker file. The tensorArena buffer for RT700 internal memory models that use the NPU must also be in noncachable memory space. The model will still run if it is in cachable memory space but the results may be incorrect.  As a side note, for non-converted models that only run on the CM33 Core0 and do not use the NPU at all (mostly only done for benchmarking comparisons) then the tensorArena can be in cachable RAM and will see better performance if it's in that cachable RAM and is located between 0x2000_0000 and 0x2058_0000 since that RAM is the main System RAM for Core0.    i.MX RT700 eIQ Neutron NPU with External Memory For large models, or in cases where RAM is limited due to other uses in the application, the model can be stored in external flash memory via XSPI0. Placing the model in the external memory has an impact on performance, however. An example of this can be found in the tflm_label_image_ext_mem example in the MCUXpresso SDK where the model is at address 0x2820_0000. When the model is in external flash, then during inference a fragmented copy of the model is done to bring in chunks of the model into the internal RAM. This does have an impact on performance of the model and an example is given in the app note. Note: If placed in external memory then the --fetch_constants_to_sram option must be used during NPU conversion of the model to let the Neutron library know that it needs to do this fragmented copy during inference.      The scratch_weights buffer size required for this operation is printed out in the Scratch field during the model conversion when using the required --fetch-constants-to-sram argument:   And the scratchWeightsBuffer is created in the \eiq\tensorflow-lite\tensorflow\lite\micro\kernels\neutron\neutron.cpp file and the size can be modified by editing: #define SCRATCH_WEIGHTS_SRAM_SIZE  1200*1024 static uint8_t scratchWeightsBuffer[SCRATCH_WEIGHTS_SRAM_SIZE] __attribute__((aligned(16))) __attribute__((section("NonCacheable")));   If the scratch memory buffer size is too small for the model then there will not be an error message but the model output may be incorrect.  Also note that the Scratch Memory buffer is only needed when running a Neutron enabled model in external memory on i.MX RT700. If using a non-Neutron enabled model that only uses the CM33 core to run, then it is not needed. 
View full article
Recovery Methods for RT595 and RT685 Development Boards When Programming Fails During the development and use of RT595 and RT685 development boards, developers often encounter a common issue reported by users: persistent errors during programming via a debugger, making it impossible to reprogram the board and effectively rendering it “bricked.” These issues can arise from various causes, such as incorrect FCB writing, interruptions during the download process, or other unknown anomalies. This article introduces two effective recovery methods: Using the SEC TOOL utility. Using an external J-Link programmer. Note: Both methods require setting the RT595 and RT685 boards to Serial ISP mode beforehand. NXP has released two RT685-based development boards (MIMXRT685-AUD-EVK and MIMXRT685-EVK) and one RT595 board. Since the RT595 board operates similarly to the RT685 boards, this article uses the MIMXRT685-AUD-EVK board for demonstration. Ensure the SDK version is correct during the process. 1. Preparation: Entering Serial ISP Mode Using the MIMXRT685-AUD-EVK board as an example, set switches SW5[1-3] to “ON OFF OFF” to enter Serial ISP mode. This corresponds to the following pin levels: PIO1_17: High PIO1_16: High PIO1_15: Low Refer to the RT600 User Manual for detailed mappings between ISP pins and boot modes.   2. Method 1: Recovery Using SEC TOOL  1. Preparation: Generate APP Image Import SDK Demo: Open MCUXpresso IDE and import the demo project mimxrt685audevk_lpc_gpio_led_output_cm33.   Modify Project Settings: Make two key configuration changes to ensure successful image generation. Generate Hex File: After configuration, build the project to generate a Hex file for use with SEC TOOL. 2. Using SEC TOOL Download SEC TOOL: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING Create Workspace: Launch SEC TOOL and create a new workspace for MIMXRT685S. Select Connection Method: RT500 and RT600 support USB, UART, SPI, and I2C. Choose one (e.g., UART via J5 or USB via J7). Only one protocol can be used at a time. If switching, power cycle the board. Configure Flash Type and Test: Select the default external NOR Flash for MIMXRT685-AUD-EVK, apply settings, and run a test. Build Image: Use the previously generated App image and click “Build Image.”    Program Image: Flash the image to the RT685 chip.   Switch Boot Mode: Power off the board and set Boot mode to FlexSPI Boot from PortB: PIO1_17: Low PIO1_16: High PIO1_15: Low SW5[1-3]: “ON OFF ON” Power on the board again. It should now operate normally and run the program successfully. 3. Method 2: Recovery Using J-Link Programmer 1. Preparation: Generate Flashable File Import the same demo project into MCUXpresso IDE and compile it without modifications to generate a Hex or S19 file. Download and install SEGGER J-Flash from SEGGER Official Website. 2. Hardware Setup Board Modifications: Connect pins 2 and 3 of JP2. Remove jumpers JP17, JP18, JP19 (ensure p3 is disconnected). Set SW5 to “ON OFF OFF”. Device Connection: Connect J-Link Plus to J19 on the board. Connect J6 to the PC to power the board. 3. Programming with J-Flash Create New Project: Open J-Flash and create a new project for MIMXRT685S. Note: RT685 supports only SWD, not JTAG. Flash Program: Load the Hex file and flash it to the board.   Switch Boot Mode: After flashing, power off the board and set Boot mode to FlexSPI Boot from PortB: PIO1_17: Low PIO1_16: High PIO1_15: Low SW5[1-3]: “ON OFF ON” Power on the board again. It should now function normally and run the program successfully.   Conclusion By following either of the two methods described above, developers can effectively recover RT595 and RT685 development boards from programming failures and restore normal operation. Choose the method that best suits your specific situation. 
View full article
This is a guide line to run both the master core and slave core projects as XIP targets from one flash.
View full article
1. Abstract The GenAVB/TSN Stack FreeRTOS Evaluation User's Guide (version:8.0 Release) covers multiple hardware platforms, software configurations, and evaluation use cases. While comprehensive, the document can be challenging for first-time users to follow due to the large amount of information and the variety of supported scenarios. This article focuses on a specific use case from the User's Guide and provides a detailed, step-by-step walkthrough with screenshots, configuration examples, expected results, and troubleshooting tips. The goal is to help users better understand the setup process and successfully evaluate the GenAVB/TSN stack on NXP platforms. This article walks through Section 4.4, TSN Network Only with TSN Bridge and Standalone Endpoint i.MX RT1180, from the GenAVB/TSN Stack FreeRTOS Evaluation User's Guide. It explains the required hardware setup, firmware build and flashing procedure, board configuration, TSN configuration, execution steps, expected results, and basic troubleshooting tips. 2. Setup 2.1 Hardware Preparation Two i.MX RT1180 boards A PC with a serial terminal emulator. MobaXterm Portable is recommended. At least two USB cables and three Ethernet cables   2.2 Firmware Preparation 2.2.1 Setup IDE and SDK Refer to the NXP GenAVB/TSN MCUXpresso User's Guide to install the required software environment for the selected platform and project. A successful project build confirms that the build environment has been installed and configured correctly. VS Code and MCUXpresso for Visual Studio Code are recommended. 2.2.2 Build Image Note:  The specific operating procedures should still be based on GenAVB/TSN MCUXpresso User's Guide . The explanation below is intended only as a supplement to the original document. For GenAVB_TSN-rtos-apps version 8.0, the CM7 Kconfig file needs to be fixed manually before building the image. Kconfig file path:   Add two lines like the following: Set the Build Configurations of the CM33 project to release_no_enetc0, and then build the project. Set the Build Configurations of the CM7 project to release_enetc0, and then build the project. Note: If you are using MCUXpresso for VS Code, you may not be able to import both the CM33 and CM7 projects of the TSN application into the same workspace at the same time, like the following: If this occurs, remove the existing project from the workspace before importing the project for the other core. This issue is expected to be fixed in a future release. After both the CM33 and CM7 projects are built successfully, the generated .bin files and .elf files can be found in the corresponding output directories:   2.2.3 Flash Image Make sure the board's boot configuration switch is set to Serial Downloader mode. For SDP mode, SW5[1..4] should be set to 0001. Set jumper J1 to position 7–8 so that the evaluation board can be powered through the Debug USB port. Connect one USB cable between the PC and the USB_OTG1 port , which is used for firmware downloading. Connect another USB cable between the PC and the Debug USB port, which is used for power supply and serial communication. Then reset the board. Refer to Chapter 10, "Multi core (Cortex-M33 + Cortex-M7) images flashing" in the GenAVB/TSN MCUXpresso User's Guide. Flash the following generated binaries to the target device: genavb_tsn_rtos_apps\...\release_no_enetc0\evkmimxrt1180_tsn_app_cm33_cm33.bin genavb_tsn_rtos_apps\...\release_enetc0\evkmimxrt1180_tsn_app_cm7_cm7.bin 2.3 Check the Status of the Boards After the flashing operation is completed on both boards, restore the boot configuration switch on each board to Quad SPI mode. For QSPI mode, SW5[1..4] should be set to 0100. Then reset both boards. Remove the jumper on JP7 so that the debug port on each board can enumerate two serial ports. The CM33 and CM7 serial terminal interfaces are provided through the two serial ports enumerated by the debug port. After the boards restart, the red LED D7 should blink, indicating that the TSN application is running. Then, check the hardware connection:     2.4 TSN Configuration and Evaluation   i.MX RT1180 Controller i.MX RT1180 IO Device 1 Step 1. Configure the Controller Standalone TSN Endpoint and IO Device Standalone TSN Endpoint respectively. CM33 shell: Press INSERT key mkdir -p /m7/tsn_app write /m7/boot 1 write /m7/tsn_app/role 0 write /m7/tsn_app/mode 2 write /m7/tsn_app/port_id 1 write /m7/tsn_app/num_io_devices 1 write /m7/tsn_app/period_ns 250000 CM33 shell: Press INSERT key mkdir -p /m7/tsn_app write /m7/boot 1 write /m7/tsn_app/role 1 write /m7/tsn_app/mode 2 write /m7/tsn_app/port_id 1 write /m7/tsn_app/period_ns 250000   Step 2. Reset the boards Reset Reset Step 3. Set hardware address CM33 shell: mkdir -p port0 mkdir -p port1 mkdir -p port2 mkdir -p port3 mkdir -p port4 mkdir -p port5 write port0/hw_addr 54:27:8D:00:00:00 write port1/hw_addr 54:27:8D:00:00:01 write port2/hw_addr 54:27:8D:00:00:02 write port3/hw_addr 54:27:8D:00:00:03 write port4/hw_addr 54:27:8D:00:00:04 write port5/hw_addr 54:27:8D:00:00:05 CM33 shell: mkdir -p port0 mkdir -p port1 mkdir -p port2 mkdir -p port3 mkdir -p port4 mkdir -p port5 write port0/hw_addr 54:27:8D:00:01:00 write port1/hw_addr 54:27:8D:00:01:01 write port2/hw_addr 54:27:8D:00:01:02 write port3/hw_addr 54:27:8D:00:01:03 write port4/hw_addr 54:27:8D:00:01:04 write port5/hw_addr 54:27:8D:00:01:05 Step 4. Set gPTP / (Devices without this command configured remain GM devices.)   CM33 shell: mkdir -p fgptp write fgptp/priority1 248   Step 5. VLAN and FDB entry settings BRIDGE>> vlan_update 2 3 -c 1 -p BRIDGE>> vlan_update 2 4 -c 1 -p BRIDGE>> fdb_update 91:e0:f0:00:fe:70 2 4 -c 1 -p BRIDGE>> fdb_update 91:e0:f0:00:fe:71 2 3 -c 1 -p /   Step 6. Scheduled Traffic settings CM33 shell:   BRIDGE>> cd / BRIDGE>> qbv_set 4 -b 35000 -c 250000 -C 0 -l 08,80000 -l f7,170000 -p BRIDGE>> qbv_set 3 -b 160000 -c 250000 -C 0 -l 08,80000 -l f7,170000 -p   CM7 shell:   CONTROLLER>> qbv_set 1 -b 35000 -c 250000 -C 0 -l 02,80000 -l fd,170000 CM7 shell:   IO_DEVICE_0>> qbv_set 1 -b 160000 -c 250000 -C 0 -l 02,80000 -l fd,170000 Step 7. Reset the boards and evaluate Scheduled Traffic /   Step 8. Configure Time-Specific Departure (TSD) CM33 shell: Press INSERT key   write /m7/tsn_app/tx_time_enabled 1 write /m7/tsn_app/tx_time_offset_ns 38000 CM33 shell: Press INSERT key   write /m7/tsn_app/tx_time_enabled 1 write /m7/tsn_app/tx_time_offset_ns 38000 Step 9. Reset the boards and evaluate Time-Specific Departure (TSD) /   Note: All use cases require the hardware address and gPTP configurations. The original User's Guide does not fully describe this part, so these steps are explicitly included in this article for clarity. 3. Conclusion This guide summarizes the complete workflow for evaluating the GenAVB/TSN Stack FreeRTOS use case on the i.MX RT1180 platform. It covers the required hardware preparation, firmware build process, image flashing procedure, board boot configuration, serial port verification, and TSN configuration steps. By following the configuration sequence in this document, users can set up the Controller and IO Device roles, configure gPTP, VLAN, FDB entries, Scheduled Traffic, and Time-Specific Departure, and then verify the expected TSN behavior between the two i.MX RT1180 boards.
View full article
This article describes the end-to-end procedure for booting a non-XIP application from SEMC parallel NAND flash on the MIMXRT1170-EVKB.
View full article
Zephyr now supports the eIQ Neutron NPU on MCX N and i.MX RT700. This article will describe how to get Zephyr and use the eIQ Neutron NPU libraries and examples.  Some previous experience with eIQ Neutron NPU enablement is assumed, so ensure you're familiar with the eIQ Neutron SDK, converting models for eIQ Neutron NPU, and basic ML concepts by going through the MCX N or i.MX RT700  NPU bare-metal lab guides for VS Code before continuing on below.  Install Software Run the MCUXpresso Installer tool and install three key components: Zephyr Developer Arm GNU Toolchain Zephyr SDK LinkServer   Install LinkServer and add LinkServer to the PATH Install VS Code and MCUxpresso VS Code plugin   Download Zephyr Open VSCode Go to the MCUXpresso for VSCode plugin and click on Import Repository Go to the Remote tab and select the Zephyr repository. Choose it a directory name and location to download the repository to, and then click on Import.   It will take approximately 30 minutes to download the repository. Near the end of the download there will be several prompts in the terminal asking to accept licenses. Type “y” to accept and hit enter. There will be about 10 of these prompts at the end. Open the MCUXpresso Venv Terminal which has a Python virtual environment with all the paths preconfigured that were installed by MCUXpresso Installer.   In the terminal that pops up, type “1” to select the default environment. Then navigate to the directory you downloaded Zephyr into Run the following commands to get TensorFlow: west config manifest.project-filter -- +tflite-micro west update Go into the zephyr subdirectory folder cd zephyr Now need to explicitly download the Pull Request (PR) that enables eIQ Neutron. This eventually won’t be necessary when Zephyr 4.5 is released in October, but until then will need to type the following In the command prompt to get it:   git remote -v git remote add upstream https://github.com/zephyrproject-rtos/zephyr.git git remote -v   git stash git fetch upstream pull/108834/head:pr-108834 git checkout pr-108834   After this command you should see there’s now a folder at <zephyr_location>\ \zephyr\samples\boards\nxp\tflm_neutron with example source code.   Compile and Run a Zephyr eIQ Neutron NPU example Compile the project with west:  For MCX N: west build -p auto -b frdm_mcxn947/mcxn947/cpu0 samples/boards/nxp/tflm_neutron   For RT700: west build -p auto -b mimxrt700_evk/mimxrt798s/cm33_cpu0 samples/boards/nxp/tflm_neutron Open TeraTerm or other serial terminal program, and connect to the virtual COM port that board enumerated as when you plugged in the USB cable. Use 115200 baud, 1 stop bit, no parity. Flash the resulting code with west flash The serial terminal should show the following: Can debug with west debug      Run your own NPU accelerated ML model in Zephyr Make sure you've gone through the MCX N or i.MX RT700  hands-on labs so you're familiar with the enablement. The same steps for converting a model with the Neutron Compiler tool inside eIQ Neutron SDK, updating the eIQ Neutron libraries, modfiying the operator list, and adding a new model are relevant when using Zephyr, but the file locations will be Zephyr specific. Also note that the header file generated by the Neutron Compiler tool will need to be updated to match the header of the model.hpp file.  Also note that the README.rst file in the Zephyr Neutron example mentions using eIQ Toolkit but that information is outdated and been superseded by eIQ Neutron SDK.  eIQ Neutron example is at <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron Neutron libraries are at <zephyr_location>\modules\hal\nxp\zephyr\blobs\neutron\ Model data is at <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\models\mcxn\model.hpp Labels file is at <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\labels.h kTensorArenaSize variable is set in <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 40) and is set to 60KB by default OpResolver is set in <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 65) The model is selected in <zephyr_location>\zephyr\samples\boards\nxp\tflm_neutron\src\main_functions.cpp (line 11)   Additional References: Blog post on west which Zephyr uses. Zephyr on FRDM-MCXN947 Zephyr on i.MX RT700 Zephyr TensorFlow
View full article
ModelRunner is a benchmarking tool for running TensorFlow Lite models on NXP microcontrollers. It supports both HTTP and UART communication modes and provides detailed latency profiling for each model layer. The model profiling information is in JSON format and can be uploaded to the upcoming eIQ AI Toolkit and eIQ AI Hub tools for more detailed analysis.  ModelRunner is available on the following MCU devices: FRDM-MCXN947 MCX-N5XX-EVK MCX-N9XX-EVK MIMXRT700-EVK MIMXRT595-EVK MIMXRT685-EVK MIMXRT1060-EVK MIMXRT1170-EVK There are two methods for using ModelRunner: Via an Ethernet connection to the board Via UART using an emulated network connection  - useful for devices without Ethernet like i.MX RT700   The attached guide walks through how to use both methods. A Windows Powershell or Linux prompt should be used for this lab as a normal Windows command prompt will not parse the commands correctly.   
View full article
i.MX RT1170 MCUboot-Custom ECDSA Keys and Direct-XIP OTA Validation Abstract This article uses the MIMXRT1170-EVKB platform to demonstrate how to generate a custom ECDSA-P256 key pair for MCUboot, replace the default public key in the mcuboot_opensource project, and re-sign application images with the new private key. It then uses the Shell and XMODEM functions provided by ota_mcuboot_basic to transfer a candidate image to the Secondary Slot. MCUboot performs signature verification, image-state checks, and version selection, and uses Flash Remap to support Direct-XIP execution. The results show that an image signed with the old key cannot be verified by the new public key, while a higher-version LED image signed with the new private key can be written to the Secondary Slot and started directly through Flash Remap. Important: The addresses, slot sizes, and commands in this article apply to the RT1170 example project used in this validation. Before porting the procedure to another project, verify the linker script, Flash partitioning, and MCUboot configuration. 1. Why Replace the Default Signing Key? The MCUboot example key included in the NXP MCUXpresso SDK is intended for development and validation only. Because it is publicly available, it is not suitable for production releases. For production, the release owner should securely protect the private key and compile only the corresponding public key into the bootloader. After the public key is replaced, images signed with the old private key should fail signature verification, confirming that the new key has taken effect. Signature verification, version management, and image confirmation serve different purposes—ensuring a trusted source, selecting an upgrade image, and managing runtime state, respectively—and cannot replace one another. 2. Platform Configuration and Scope 3. Flash Layout  Each signed image contains a 0x400-byte MCUboot header that records boot metadata such as the image size and version. At power-on, MCUboot checks the images in both slots, parses the header and TLV area, verifies image integrity and the ECDSA signature, and evaluates image state and version. In the test configuration used here, images are generated with --confirm. Among images that satisfy the signature and state requirements, MCUboot selects the higher version that complies with the upgrade policy. This behavior applies only to this test configuration and does not represent every MCUboot state or upgrade policy. In DIRECT-XIP + FLASH REMAP mode, if the selected image is stored in the non-default mapped slot, MCUboot configures Flash Remap before jumping to the application. This maps the image's physical storage region to the logical execution address expected by the application, allowing in-place execution without copying or swapping images. 4. MCUboot Signature Verification Fundamentals Important: A hash detects content changes; a digital signature verifies image origin and integrity; the version number identifies and compares image releases; and the Confirm state determines whether a test image is retained permanently. 5. Generate an ECDSA-P256 Private Key in the scripts Directory imgtool.py is located in the middleware\mcuboot_opensource\scripts directory of the MCUXpresso SDK. Change to this directory before running the key-generation command. Replace <SDK_INSTALL_PATH> with the actual SDK installation path on your computer: <SDK_INSTALL_PATH>\middleware\mcuboot_opensource\scripts python imgtool.py keygen ^  -k my_priv.pem ^  -t ecdsa-p256 dir my_priv.pem keygen: Generates a new key. -k my_priv.pem: Specifies the output key file. -t ecdsa-p256: Selects the ECDSA-P256 algorithm. After the command completes successfully, the private key is generated as middleware\mcuboot_opensource\scripts\my_priv.pem. Security reminder: In a production project, never compile the private key into the bootloader, program it into the MCU, commit it to a regular Git repository, or distribute it with the SDK project. Store only the public key in the bootloader. 6. Export and Replace the MCUboot Public Key python imgtool.py getpub -k my_priv.pem python imgtool.py getpub -k my_priv.pem > my_pub.c The command outputs a C array that can be compiled by MCUboot. The key symbols are: const unsigned char ecdsa_pub_key[] = {     0x30, 0x59, ... }; const unsigned int ecdsa_pub_key_len = 91; The public-key source file replaced in this article is: evkbmimxrt1170_mcuboot_opensource_cm7\bootutil\nxp_port\keys\sign-ecdsa-p256-pub.c Back up the original public-key file, and do not include the backup copy in the project build. Replace the original public-key array with the output from getpub. Keep the ecdsa_pub_key and ecdsa_pub_key_len symbol names consistent with the project references. Clean and rebuild evkbmimxrt1170_mcuboot_opensource_cm7. Program the new bootloader at 0x30000000. 7. Negative Validation: Images Signed with the Old Key Are Rejected Replace only the signature-verification public key in MCUboot, rebuild and program the updated bootloader, and leave the existing application image in Flash without re-signing it with the new private key. Because the image is still signed with the old private key while MCUboot now verifies it with the new public key, the key pair does not match. The image therefore fails signature verification and is classified as invalid. In the project configuration used here, the bootloader then erases the invalid image. This negative test confirms that the new public key has been compiled into MCUboot correctly and is actively used during boot verification. If the image signed with the old key is classified as invalid, the new public key has been compiled correctly and is being used for MCUboot verification. Successfully parsing the image header and reading the version only proves that the image structure is recognizable; it does not mean signature verification passed. A digital signature generated with the old private key cannot be verified by a nonmatching new public key. The version number is used only for image identification and upgrade selection. It cannot replace signature verification; even an image with a correct or higher version will not boot if signature verification fails. 8. Sign the ota_mcuboot_basic Image with the New Private Key python imgtool.py sign ^  --key my_priv.pem ^  --align 4 ^  --version 1.4.0 ^  --slot-size 0x200000 ^  --header-size 0x400 ^  --pad-header ^  --pad ^  --confirm ^  evkbmimxrt1170_ota_mcuboot_basic_cm7.bin ^  ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin evkbmimxrt1170_ota_mcuboot_basic_cm7.bin is the raw application image generated by the Basic project. In this example, --confirm is added so that the image is generated with the Confirmed state. Note the following: Notes on --confirm and Production Deployment The README states that an initial image manually programmed together with the bootloader requires the additional --pad and --confirm options. Otherwise, the bootloader may reject the image because the trailer lacks the required state information. --pad pads the image to the size specified by --slot-size and creates the slot trailer required by MCUboot. --confirm presets the image_ok flag in the trailer to the confirmed state while the image is generated. MCUboot therefore treats the initial image as a confirmed valid image at boot. Production recommendation: This usage is intended mainly for the initial image manually programmed together with the bootloader. It is not recommended for production OTA images. Pre-confirming an update image with --confirm bypasses MCUboot's test boot → image confirmation → failure rollback flow. If the new image cannot boot, fails peripheral initialization, or encounters a critical application error, MCUboot cannot use the unconfirmed state to roll back automatically, which may leave the device unrecoverable. The MCUboot bootloader primarily reads the image_ok flag in the trailer and uses it for image-state evaluation, version selection, and rollback handling. It does not proactively write the confirmation flag on behalf of the application. The running application should explicitly confirm the image at an appropriate time. For example, after the candidate application completes its startup self-test, peripheral initialization, and critical functional checks, it can call boot_set_confirmed(). An application with Shell support, such as ota_mcuboot_basic, can also be confirmed manually with the image accept command. This preserves MCUboot's test-boot and failure-rollback capabilities and prevents a faulty image from being marked permanently valid too early.   python imgtool.py dumpinfo ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin Check the magic, hdr_size, img_size, version, and TLV information in the output. The TLV area should contain SHA256, KEYHASH, and ECDSASIG, which represent the image digest, public-key identifier, and ECDSA signature respectively. 9. Program the Signed ota_mcuboot_basic Image into the Primary Slot This article uses ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin, generated in the previous section, as the initial image in the Primary Slot. ota_mcuboot_basic provides the Shell and XMODEM image-receive functions. After it starts, the application can transfer subsequent candidate images to the Secondary Slot. Program the signed image containing the complete MCUboot header, application payload, and signature TLV—not the raw BIN generated directly by the application project. File to program: ota_mcuboot_basic_1_4_0_confirmed.SIGNED.bin Programming address: 0x30040000 Program the complete signed image at the Primary Slot start address, 0x30040000. Reset the device and inspect the MCUboot log to confirm that signature verification succeeds and the version is read correctly. Confirm that the device enters the ota_mcuboot_basic Shell and that image info reports the image state. 10. Generate a Candidate Signed Image for the Secondary Slot This article creates an LED application project and uses it as the candidate image for the Secondary Slot. The image is signed with the newly generated private key, my_priv.pem, and assigned a version later than the currently running image. In DIRECT-XIP + FLASH REMAP mode, both the LED and ota_mcuboot_basic projects are linked to the same logical addresses: the signed image begins logically at 0x30040000, and the application vector table is at 0x30040400. The signed LED image is physically written to the Secondary Slot at 0x30240000, with its vector table physically located at 0x30240400. When MCUboot selects this image, Flash Remap maps the Secondary Slot to the logical execution address expected by the application. Therefore, the Secondary Slot identifies the image's physical storage location, while the application still executes using the logical addresses associated with the Primary Slot. python imgtool.py sign ^  --key my_priv.pem ^  --align 4 ^  --version 1.5.0 ^  --slot-size 0x200000 ^  --header-size 0x400 ^  --pad-header ^  --pad ^  --confirm ^  evkbmimxrt1170_igpio_led_output_cm7_second_app.bin ^  ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin --key my_priv.pem: Uses the private key paired with the public key currently trusted by MCUboot. --version 1.5.0: Sets the candidate image version, which must be later than the currently running version 1.4.0. --slot-size 0x200000: Matches the slot size in the current Flash partition layout. --header-size 0x400 and --pad-header: Reserve and populate the 0x400-byte MCUboot header area at the beginning of the image. --pad: Pads the output to the full size specified by --slot-size and reserves the image trailer area. Whether the image is pre-confirmed is controlled by --confirm. --confirm: Generates the candidate image in the Confirmed state. python imgtool.py dumpinfo ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin Before transfer, verify that the output reports valid magic, hdr_size, img_size, version, and TLV information. In particular, confirm that the version is 1.5.0+0 and that the TLV area contains SHA256, KEYHASH, and ECDSASIG. After the checks pass, use the complete ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin file in the next section. The ota_mcuboot_basic application transfers it to the Secondary Slot through XMODEM. 11. Transfer the Signed Image to the Secondary Slot Using XMODEM Start the development board, enter the Basic Shell, and run the xmodem command. In the serial terminal, select File → Transfer → XMODEM, select ota_led_output_second_app_1_5_0_confirmed.SIGNED.bin, and start the transfer. After the transfer completes, run image info and verify the version and image state in the Secondary Slot. 12. Inspect the Candidate Image and Validate Version Switching image info reboot After reboot, inspect the MCUboot log for the Primary and Secondary versions, confirmation states, and selected boot slot. In the test configuration used here, the candidate image is pre-confirmed with --confirm. It must pass signature verification, satisfy the Confirmed-state requirements, and have a later version that complies with the upgrade policy. A valid signature means only that the image source is trusted and the content is intact; it does not guarantee that the image will be selected. Once all conditions are met, MCUboot boots the candidate image. In Direct-XIP + Flash Remap mode, the image can execute in place from the Secondary Slot without being copied or swapped. 13. Summary Generate and securely store a project-specific ECDSA-P256 private key, and compile the corresponding public key into the MCUboot project. Confirm that key replacement is effective by verifying that images signed with the old key fail while images signed with the new private key pass. Use the signed ota_mcuboot_basic image as the initial Primary Slot image and the later-version signed LED image as the Secondary Slot update image. Transfer the complete signed image to the Secondary Slot through XMODEM and validate the MCUboot flow that starts the update image through Flash Remap. For production OTA, remove --confirm and have the application write image_ok by calling boot_set_confirmed() after successful self-tests, preserving MCUboot's automatic rollback capability.
View full article
OEM Key Import, Signed Message, and TLV Blob Generation Flow  Based on the i.MX RT1180 EdgeLock Enclave 
View full article