yocto package generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto package generation

1,269 Views
ronjacoby1
Contributor I

hi,

generating the imx-image-full for iMX8, it seems that the different deb files are generated each time i run the full build, after deleting tmp folder.

for example, i used  packagegroup-fsl-gstreamer1.0-base, and it was not created after a rebuild. i made no change to local.conf

0 Kudos
Reply
1 Reply

1,219 Views
Harvey021
NXP TechSupport
NXP TechSupport

Hi @ronjacoby1 

It should be no such difference when no changes to build configuration or environments, such as change the target MACHINE? Or do repo sync on the basis of internal xml? 

 

Best regards

Harvey

0 Kudos
Reply