yocto L4.1.15 bitbake mfgtool-initramfs command failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto L4.1.15 bitbake mfgtool-initramfs command failed

3,075件の閲覧回数
m_c
Senior Contributor I

$ bitbake fsl-image-mfgtool-initramfs

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2825 entries from dependency cache.

Parsing recipes: 100% |#########################################| Time: 00:00:00

Parsing of 2258 .bb files complete (2242 cached, 16 parsed). 2824 targets, 448 skipped, 5 masked, 0 errors.

NOTE: Resolving any missing task queue dependencies

Build Configuration:

BB_VERSION        = "1.28.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-14.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabresd"

DISTRO            = "fsl-imx-fb"

DISTRO_VERSION    = "4.1.15-1.1.1"

TUNE_FEATURES     = "arm armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta

meta-yocto        = "HEAD:dd0ba9ea4a11ab15348d4fe3574e4b28784db82f"

meta-oe

meta-multimedia   = "HEAD:ad6133a2e95f4b83b6b3ea413598e2cd5fb3fd90"

meta-fsl-arm      = "HEAD:35b8b9bd9863de208ab60e33b55f10ee43e2619b"

meta-fsl-arm-extra = "HEAD:e200df91b70da254461c59082ddd5db0a3c415a2"

meta-fsl-demos    = "HEAD:2231e946e7a94d096394f2b2477e8184c9bbde7b"

meta-bsp

meta-sdk          = "HEAD:f39f40c71ce4511029c56e6d57aa48bd172124d3"

meta-browser      = "HEAD:b6d46d69a261fe6bd7c1e9811dc2a9bbd0b79aeb"

meta-gnome

meta-networking

meta-python

meta-ruby

meta-filesystems

meta-xfce         = "HEAD:ad6133a2e95f4b83b6b3ea413598e2cd5fb3fd90"

meta-qt5          = "HEAD:d5536e34ec985c82b621448ab4325e5cbba38560"

NOTE: Preparing RunQueue

WARNING: /home/mike/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx-mfgtool_4.1.15.bb.do_compile is tainted from a forced run

WARNING: /home/mike/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-kernel/linux/linux-imx-mfgtool_4.1.15.bb.do_deploy is tainted from a forced run

WARNING: /home/mike/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx-mfgtool_2015.04.bb.do_compile is tainted from a forced run

WARNING: /home/mike/yocto/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx-mfgtool_2015.04.bb.do_deploy is tainted from a forced run

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

ERROR: Index creation command '/home/mike/yocto/imx6qsabresd/tmp/sysroots/x86_64-linux/usr/bin/createrepo --dbpath /home/mike/yocto/imx6qsabresd/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-mfgtool-initramfs/1.0-r0/rpmdb/all --update -q /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/all' failed with return code 1:

Error moving final /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/all/repodata to old dir /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/all/.olddata

Index creation command '/home/mike/yocto/imx6qsabresd/tmp/sysroots/x86_64-linux/usr/bin/createrepo --dbpath /home/mike/yocto/imx6qsabresd/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-mfgtool-initramfs/1.0-r0/rpmdb/imx6qsabresd --update -q /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/imx6qsabresd' failed with return code 1:

Error moving final /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/imx6qsabresd/repodata to old dir /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/imx6qsabresd/.olddata

Index creation command '/home/mike/yocto/imx6qsabresd/tmp/sysroots/x86_64-linux/usr/bin/createrepo --dbpath /home/mike/yocto/imx6qsabresd/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-mfgtool-initramfs/1.0-r0/rpmdb/cortexa9hf_vfp_neon --update -q /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/cortexa9hf_vfp_neon' failed with return code 1:

Error moving final /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/cortexa9hf_vfp_neon/repodata to old dir /home/mike/yocto/imx6qsabresd/tmp/deploy/rpm/cortexa9hf_vfp_neon/.olddata

ERROR: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/mike/yocto/imx6qsabresd/tmp/work/imx6qsabresd-poky-linux-gnueabi/fsl-image-mfgtool-initramfs/1.0-r0/temp/log.do_rootfs.153

ERROR: Task 7 (/home/mike/yocto/sources/meta-fsl-arm/recipes-fsl/images/fsl-image-mfgtool-initramfs.bb, do_rootfs) failed with exit code '1'

NOTE: Tasks Summary: Attempted 1478 tasks of which 1477 didn't need to be rerun and 1 failed.

No currently running tasks (1477 of 1479)

Summary: 1 task failed:

  /home/mike/yocto/sources/meta-fsl-arm/recipes-fsl/images/fsl-image-mfgtool-initramfs.bb, do_rootfs

Summary: There were 4 WARNING messages shown.

ラベル(1)
0 件の賞賛
返信
1 返信

1,830件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I tried the following :

$ mkdir fsl-release-bsp

$ cd fsl-release-bsp

$ repo init -u git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-4.1.15-1.0.0_ga

$ repo sync

$ DISTRO=fsl-imx-x11 MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-x11

$ bitbake fsl-image-gui

$ bitbake fsl-image-mfgtool-initramfs

It works !

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信