wm8985 audio codec support in imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

wm8985 audio codec support in imx6

3,417 Views
jamalmohiuddin
Contributor III

Hi Guys,

We have a custom board based on sabre sd schematic but with only one difference of audio codec. We are using wm8985 instead of wm8962 of sabre sd.

We are using linux 3.10.53 BSP generated by using buildroot.

What changes should I make to get audio work on my board.

Thanks and Regards,

Jamal

Labels (2)
Tags (2)
0 Kudos
Reply
1 Reply

3,064 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jamal

one can follow Chapter 8 Porting Audio Codecs to a Custom Board

attached Porting Gude and codec driver sources described in Chapter 29
Advanced Linux Sound Architecture (ALSA) Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply