why flash screen while using screenrecord?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

why flash screen while using screenrecord?

4,512 Views
giszxl
Contributor I

my device is imx6q. If Multiple screenrecord at the same time, the device screen is flash,as shown in the appendix below。The screen is flash while surfaceflinger has two or more virtualdisplaysurface. I found the second virtualdisplaysurface hwcId=-12. Have anyone ever met the same problem and what is the root cause?

dumpsys SurfaceFlinger info:

Build configuration: [sf] [libui] [libgui]                                                                                                                                                         
Sync configuration: [using: EGL_ANDROID_native_fence_sync EGL_KHR_wait_sync]                                                                                                                       
DispSync configuration: app phase 1000000 ns, sf phase 1000000 ns, present offset 0 ns (refresh 16949152 ns)                                                                                       
                                                                                                                                                                                                   
Static screen stats:                                                                                                                                                                               
  < 1 frames: 26.563 s (20.9%)                                                                                                                                                                     
  < 2 frames: 47.140 s (37.2%)                                                                                                                                                                     
  < 3 frames: 2.559 s (2.0%)                                                                                                                                                                       
  < 4 frames: 5.184 s (4.1%)                                                                                                                                                                       
  < 5 frames: 4.024 s (3.2%)                                                                                                                                                                       
  < 6 frames: 2.813 s (2.2%)                                                                                                                                                                       
  < 7 frames: 0.867 s (0.7%)                                                                                                                                                                       
  7+ frames: 37.721 s (29.7%)                                                                                                                                                                      
                                                                                                                                                                                                   
Buffering stats:                                                                                                                                                                                   
  [Layer name] <Active time> <Two buffer> <Double buffered> <Triple buffered>                                                                                                                      
  [com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity] 35.57 0.004 1.000 0.000                                                                                                            
  [SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity] 13.78 1.000 1.000 0.000                                                                                              
  [com.adayo.navigationbar/com.adayo.navigationbar.serviceterm.LocalPromptActivity] 0.26 0.000 1.000 0.000                                                                                         
                                                                                                                                                                                                   
Visible layers (count = 8)                                                                                                                                                                         
+ LayerDim 0xb1fce800 (animation background stackId=1)                                                                                                                                             
  Region transparentRegion (this=0xb1fcea30, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xb1fce808, count=1)                                                                                                                                                  
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region surfaceDamageRegion (this=0xb1fce844, count=1)                                                                                                                                            
    [  0,   0,   0,   0]                                                                                                                                                                           
      layerStack=   0, z=    21009, pos=(-256,-120), size=(1536, 720), crop=(   0,   0,  -1,  -1), finalCrop=(   0,   0,  -1,  -1), isOpaque=0, invalidate=0, alpha=0x00, flags=0x00000001, tr=[1.]
      client=0xb1c22000                                                                                                                                                                            
      format= 0, activeBuffer=[   0x   0:   0,  0], queued-frames=0, mRefreshPending=0                                                                                                             
            mTexName=4 mCurrentTexture=-1                                                                                                                                                          
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[1536x720], default-format=1, transform-hint=00, FIFO(0)={}  
             [00:0x0] state=FREE                                                                                                                                                                   
             [01:0x0] state=FREE                                                                                                                                                                   
             [02:0x0] state=FREE                                                                                                                                                                   
+ Layer 0xa815b400 (com.adayo.navigationbar/com.adayo.navigationbar.LuancherActivity)                                                                                                              
  Region transparentRegion (this=0xa815b630, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xa815b408, count=1)                                                                                                                                                  
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region surfaceDamageRegion (this=0xa815b444, count=1)                                                                                                                                            
    [  0,   0,   0,   0]                                                                                                                                                                           
      layerStack=   0, z=    21020, pos=(0,0), size=(1024, 480), crop=(   0,   0,1024, 480), finalCrop=(   0,   0,   0,   0), isOpaque=1, invalidate=0, alpha=0xff, flags=0x00000003, tr=[1.00, 0.]
      client=0xa8212800                                                                                                                                                                            
      format= 1, activeBuffer=[1024x 480:1024,  1], queued-frames=0, mRefreshPending=0                                                                                                             
            mTexName=5 mCurrentTexture=-1                                                                                                                                                          
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[1024x480], default-format=1, transform-hint=00, FIFO(0)={}  
             [00:0x0] state=FREE                                                                                                                                                                   
             [01:0x0] state=FREE                                                                                                                                                                   
             [02:0x0] state=FREE                                                                                                                                                                   
+ LayerDim 0xa9412000 (SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity)                                                                                                  
  Region transparentRegion (this=0xa9412230, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xa9412008, count=1)                                                                                                                                                  
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region surfaceDamageRegion (this=0xa9412044, count=1)                                                                                                                                            
    [  0,   0,   0,   0]                                                                                                                                                                           
      layerStack=   0, z=    21024, pos=(0,0), size=( 909, 480), crop=(   0,   0, 909, 480), finalCrop=(   0,   0,  -1,  -1), isOpaque=0, invalidate=0, alpha=0xff, flags=0x00000002, tr=[1.00, 0.]
      client=0xa8212a40                                                                                                                                                                            
      format= 0, activeBuffer=[   0x   0:   0,  0], queued-frames=0, mRefreshPending=0                                                                                                             
            mTexName=10 mCurrentTexture=-1                                                                                                                                                         
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[1x1], default-format=1, transform-hint=00, FIFO(0)={}       
             [00:0x0] state=FREE                                                                                                                                                                   
             [01:0x0] state=FREE                                                                                                                                                                   
             [02:0x0] state=FREE                                                                                                                                                                   
+ Layer 0xb1fcfc00 (com.android.systemui.ImageWallpaper)                                                                                                                                           
  Region transparentRegion (this=0xb1fcfe30, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xb1fcfc08, count=1)                                                                                                                                                  
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region surfaceDamageRegion (this=0xb1fcfc44, count=1)                                                                                                                                            
    [  0,   0,   0,   0]                                                                                                                                                                           
      layerStack=   0, z=    21025, pos=(0,-272), size=(1243,1024), crop=(   0,   0,1243,1024), finalCrop=(   0,   0,  -1,  -1), isOpaque=1, invalidate=0, alpha=0x00, flags=0x00000003, tr=[1.00,]
      client=0xb1c22040                                                                                                                                                                            
      format= 2, activeBuffer=[1243x1024:1248,  2], queued-frames=0, mRefreshPending=0                                                                                                             
            mTexName=3 mCurrentTexture=0                                                                                                                                                           
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[1243x1024], default-format=2, transform-hint=00, FIFO(0)={}
             [00:0x0] state=FREE                                                                                                                                                                   
             [01:0x0] state=FREE                                                                                                                                                                   
             [02:0x0] state=FREE                                                                                                                                                                   
+ Layer 0xb1fcd400 (SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity)                                                                                                     
  Region transparentRegion (this=0xb1fcd630, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xb1fcd408, count=1)                                                                                                                                                  
    [  0,   0, 909, 480]                                                                                                                                                                           
  Region surfaceDamageRegion (this=0xb1fcd444, count=1)                                                                                                                                            
    [  0,   0,   0,   0]                                                                                                                                                                           
      layerStack=   0, z=    21025, pos=(0,0), size=( 909, 480), crop=(   0,   0, 909, 480), finalCrop=(   0,   0,  -1,  -1), isOpaque=1, invalidate=0, alpha=0xff, flags=0x00000002, tr=[1.00, 0.]
      client=0xa8212a40                                                                                                                                                                            
      format= 4, activeBuffer=[ 909x 480: 912,  4], queued-frames=0, mRefreshPending=0                                                                                                             
            mTexName=9 mCurrentTexture=2                                                                                                                                                           
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[909x480], default-format=4, transform-hint=00, FIFO(0)={}   
             [00:0xa8239940] state=DEQUEUED, 0xa817f040 [ 909x 480: 912,  4]                                                                                                                       
            >[02:0xa823a840] state=ACQUIRED, 0xa817fd00 [ 909x 480: 912,  4]                                                                                                                       
             [01:0xa82399e0] state=FREE    , 0xa817f340 [ 909x 480: 912,  4]                                                                                                                       
+ Layer 0xa815dc00 (com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity)                                                                                                                   
  Region transparentRegion (this=0xa815de30, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xa815dc08, count=1)                                                                                                                                                  
    [  0,   0, 909, 480]                                                                                                                                                                           
  Region surfaceDamageRegion (this=0xa815dc44, count=1)                                                                                                                                            
    [ 95,  35, 123,  63]                                                                                                                                                                           
      layerStack=   0, z=    21030, pos=(0,0), size=(1024, 480), crop=(   0,   0, 909, 480), finalCrop=(   0,   0,  -1,  -1), isOpaque=0, invalidate=0, alpha=0xff, flags=0x00000000, tr=[1.00, 0.]
      client=0xa8212a40                                                                                                                                                                            
      format= 1, activeBuffer=[1024x 480:1024,  1], queued-frames=2, mRefreshPending=0                                                                                                             
            mTexName=7 mCurrentTexture=1                                                                                                                                                           
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[1024x480], default-format=1, transform-hint=00, FIFO(2)={02E
00:0xb1c0c6e0 crop=[0,0,0,0], xform=0x00, time=0x1ec5eeb122, scale=FREEZE                                                                                                                          
}                                                                                                                                                                                                  
             [00:0xb1c0c6e0] state=QUEUED  , 0xb1c04380 [1024x 480:1024,  1]                                                                                                                       
            >[01:0xa823a700] state=ACQUIRED, 0xa817fb80 [1024x 480:1024,  1]                                                                                                                       
             [02:0xa823a660] state=QUEUED  , 0xa817f940 [1024x 480:1024,  1]                                                                                                                       
+ Layer 0xa815c800 (StatusBar)                                                                                                                                                                     
  Region transparentRegion (this=0xa815ca30, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xa815c808, count=1)                                                                                                                                                  
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region surfaceDamageRegion (this=0xa815c844, count=1)                                                                                                                                            
    [  0,   0,   0,   0]                                                                                                                                                                           
      layerStack=   0, z=   161000, pos=(0,0), size=(1024,   1), crop=(   0,   0,  -1,  -1), finalCrop=(   0,   0,  -1,  -1), isOpaque=0, invalidate=0, alpha=0xff, flags=0x00000001, tr=[1.00, 0.]
      client=0xb1c22040                                                                                                                                                                            
      format= 1, activeBuffer=[   0x   0:   0,  0], queued-frames=0, mRefreshPending=0                                                                                                             
            mTexName=6 mCurrentTexture=-1                                                                                                                                                          
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[1024x1], default-format=1, transform-hint=00, FIFO(0)={}    
             [02:0xb1c0c8c0] state=FREE    , 0xb1c04500 [1024x   1:1024,  1]                                                                                                                       
             [01:0xb1c0c820] state=FREE    , 0xb1c04080 [1024x   1:1024,  1]                                                                                                                       
             [00:0xb1c0c780] state=FREE    , 0xb1c04140 [1024x   1:1024,  1]                                                                                                                       
+ Layer 0xa815a000 ()                                                                                                                                                                              
  Region transparentRegion (this=0xa815a230, count=1)                                                                                                                                              
    [  0,   0,   0,   0]                                                                                                                                                                           
  Region visibleRegion (this=0xa815a008, count=1)                                                                                                                                                  
    [909,   0, 1024, 480]                                                                                                                                                                          
  Region surfaceDamageRegion (this=0xa815a044, count=1)                                                                                                                                            
    [  0,   0,   0,   0]                                                                                                                                                                           
      layerStack=   0, z=   211000, pos=(909,0), size=( 115, 480), crop=(   0,   0, 115, 480), finalCrop=(   0,   0,  -1,  -1), isOpaque=0, invalidate=0, alpha=0xff, flags=0x00000000, tr=[1.00, ]
      client=0xa8212f40                                                                                                                                                                            
      format= 1, activeBuffer=[ 115x 480: 128,  1], queued-frames=0, mRefreshPending=0                                                                                                             
            mTexName=2 mCurrentTexture=0                                                                                                                                                           
            mCurrentCrop=[0,0,0,0] mCurrentTransform=0                                                                                                                                             
            mAbandoned=0                                                                                                                                                                           
            -BufferQueue mMaxAcquiredBufferCount=1, mMaxDequeuedBufferCount=2, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[115x480], default-format=1, transform-hint=00, FIFO(0)={}   
            >[00:0xa823a020] state=ACQUIRED, 0xa817e080 [ 115x 480: 128,  1]                                                                                                                       
             [02:0xa823a2a0] state=DEQUEUED, 0xa817de40 [ 115x 480: 128,  1]                                                                                                                       
             [01:0xa823a200] state=FREE    , 0xa817f100 [ 115x 480: 128,  1]                                                                                                                       
Displays (3 entries)                                                                                                                                                                               
+ DisplayDevice: NdkMediaCodec                                                                                                                                                                     
   type=2, hwcId=2, layerStack=0, (1024x 480), ANativeWindow=0xb1fff808, orient= 0 (type=00000000), flips=1553, isSecure=1, powerMode=2, activeConfig=0, numLayers=3                               
   v:[0,0,1024,480], f:[0,0,1024,480], s:[0,0,1024,480],transform:[[1.000,0.000,-0.000][0.000,1.000,-0.000][0.000,0.000,1.000]]                                                                    
+ DisplayDevice: NdkMediaCodec                                                                                                                                                                     
   type=2, hwcId=-12, layerStack=0, (1024x 480), ANativeWindow=0xa7f72008, orient= 0 (type=00000000), flips=594, isSecure=1, powerMode=2, activeConfig=0, numLayers=3                              
   v:[0,0,1024,480], f:[0,0,1024,480], s:[0,0,1024,480],transform:[[1.000,0.000,-0.000][0.000,1.000,-0.000][0.000,0.000,1.000]]                                                                    
+ DisplayDevice: Built-in Screen                                                                                                                                                                   
   type=0, hwcId=0, layerStack=0, (1024x 480), ANativeWindow=0xb1fff008, orient= 0 (type=00000000), flips=4251, isSecure=1, powerMode=2, activeConfig=0, numLayers=3                               
   v:[0,0,1024,480], f:[0,0,1024,480], s:[0,0,1024,480],transform:[[1.000,0.000,-0.000][0.000,1.000,-0.000][0.000,0.000,1.000]]                                                                    
mAbandoned=0                                                                                                                                                                                       
-BufferQueue mMaxAcquiredBufferCount=2, mMaxDequeuedBufferCount=1, mDequeueBufferCannotBlock=0 mAsyncMode=0, default-size=[1024x480], default-format=1, transform-hint=00, FIFO(0)={}              
 [00:0xa93b23c0] state=DEQUEUED, 0xb1fc3a80 [1024x 480:1024,  1]                                                                                                                                   
>[01:0xa93b25a0] state=ACQUIRED, 0xb1fc3c00 [1024x 480:1024,  1]                                                                                                                                   
 [02:0xa93e2440] state=FREE    , 0xa817d0c0 [1024x 480:1024,  1]                                                                                                                                   
SurfaceFlinger global state:                                                                                                                                                                       
EGL implementation : 1.5                                                                                                                                                                           
EGL_KHR_fence_sync EGL_KHR_reusable_sync EGL_KHR_wait_sync EGL_KHR_image EGL_KHR_image_base EGL_KHR_image_pixmap EGL_KHR_gl_texture_2D_image EGL_KHR_gl_texture_cubemap_image EGL_KHR_gl_renderbufc
GLES: Vivante Corporation, Vivante GC2000, OpenGL ES 3.0 V6.2.0.p2.79565                                                                                                                           
GL_EXT_debug_marker GL_OES_vertex_type_10_10_10_2 GL_OES_vertex_half_float GL_OES_element_index_uint GL_OES_mapbuffer GL_OES_vertex_array_object GL_OES_compressed_ETC1_RGB8_texture GL_OES_compre
  Region undefinedRegion (this=0xa93e6b6c, count=1)                                                                                                                                                
    [909,   0, 1024, 480]                                                                                                                                                                          
  orientation=0, isDisplayOn=1                                                                                                                                                                     
  last eglSwapBuffers() time: 10870.000000 us                                                                                                                                                      
  last transaction time     : 89.333000 us                                                                                                                                                         
  transaction-flags         : 00000000                                                                                                                                                             
  refresh-rate              : 59.000002 fps                                                                                                                                                        
  x-dpi                     : 159.567993                                                                                                                                                           
  y-dpi                     : 160.421005                                                                                                                                                           
  gpu_to_cpu_unsupported    : 0                                                                                                                                                                    
  eglSwapBuffers time: 3650.000000 us                                                                                                                                                              
  transaction time: 0.000000 us                                                                                                                                                                    
VSYNC state: enabled                                                                                                                                                                               
  soft-vsync: disabled                                                                                                                                                                             
  numListeners=21,                                                                                                                                                                                 
  events-delivered: 4638                                                                                                                                                                           
    0xb1c1a000: count=-1                                                                                                                                                                           
    0xb1c1a028: count=-1                                                                                                                                                                           
    0xb1c1a050: count=-1                                                                                                                                                                           
    0xb1c1a078: count=-1                                                                                                                                                                           
    0xb1c1a0a0: count=-1                                                                                                                                                                           
    0xb1c1a0c8: count=-1                                                                                                                                                                           
    0xb1c1a140: count=-1                                                                                                                                                                           
    0xb1f9c310: count=-1                                                                                                                                                                           
    0xb1f9c338: count=-1                                                                                                                                                                           
    0xb1f9c388: count=-1                                                                                                                                                                           
    0xb1f9c450: count=-1                                                                                                                                                                           
    0xb1f9c4c8: count=-1                                                                                                                                                                           
    0xb1f9c540: count=-1                                                                                                                                                                           
    0xb1f9c568: count=-1                                                                                                                                                                           
    0xb1f9c590: count=-1                                                                                                                                                                           
    0xb1f9c6a8: count=-1                                                                                                                                                                           
    0xb1f9c6f8: count=-1                                                                                                                                                                           
    0xb1f9c8d8: count=-1                                                                                                                                                                           
    0xb1f9cc20: count=-1                                                                                                                                                                           
    0xb1f9cc70: count=-1                                                                                                                                                                           
    0xb1f9cc98: count=-1                                                                                                                                                                           
h/w composer state:                                                                                                                                                                                
  h/w composer present and enabled                                                                                                                                                                 
Hardware Composer state (version 01030000):                                                                                                                                                        
  mDebugForceFakeVSync=0                                                                                                                                                                           
  Display[0] configurations (* current):                                                                                                                                                           
    * 0: 1024x480, xdpi=159.567993, ydpi=160.421005, refresh=16949152, colorMode=0                                                                                                                 
  numHwLayers=4, flags=00000000                                                                                                                                                                    
    type   |  handle  | hint | flag | tr | blnd |   format    |     source crop (l,t,r,b)      |          frame         | name                                                                     
-----------+----------+------+------+----+------+-------------+--------------------------------+------------------------+------                                                                    
       HWC | a817fd00 | 0000 | 0000 | 00 | 0100 | RGB_565     |    0.0,    0.0,  909.0,  480.0 |    0,    0,  909,  480 | SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity
       HWC | a817f940 | 0000 | 0000 | 00 | 0105 | RGBA_8888   |    0.0,    0.0,  909.0,  480.0 |    0,    0,  909,  480 | com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity              
       HWC | a817e080 | 0000 | 0000 | 00 | 0105 | RGBA_8888   |    0.0,    0.0,  115.0,  480.0 |  909,    0, 1024,  480 |                                                                          
 FB TARGET | b1fc3c00 | 0000 | 0000 | 00 | 0105 | RGBA_8888   |    0.0,    0.0, 1024.0,  480.0 |    0,    0, 1024,  480 | HWC_FRAMEBUFFER_TARGET                                                   
  Display[2] configurations (* current):                                                                                                                                                           
    * 0: 1024x480, xdpi=213.000000, ydpi=213.000000, refresh=4294967040, colorMode=0                                                                                                               
  numHwLayers=4, flags=00000000                                                                                                                                                                    
    type   |  handle  | hint | flag | tr | blnd |   format    |     source crop (l,t,r,b)      |          frame         | name                                                                     
-----------+----------+------+------+----+------+-------------+--------------------------------+------------------------+------                                                                    
       HWC | a817fd00 | 0000 | 0000 | 00 | 0100 | RGB_565     |    0.0,    0.0,  909.0,  480.0 |    0,    0,  909,  480 | SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity
       HWC | a817f940 | 0000 | 0000 | 00 | 0105 | RGBA_8888   |    0.0,    0.0,  909.0,  480.0 |    0,    0,  909,  480 | com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity              
       HWC | a817e080 | 0000 | 0000 | 00 | 0105 | RGBA_8888   |    0.0,    0.0,  115.0,  480.0 |  909,    0, 1024,  480 |                                                                          
 FB TARGET | a817fa00 | 0000 | 0000 | 00 | 0105 | RGBA_8888   |    0.0,    0.0, 1024.0,  480.0 |    0,    0, 1024,  480 | HWC_FRAMEBUFFER_TARGET                                                   
Allocated buffers:                                                                                                                                                                                 
0xa817d0c0: 1920.00 KiB | 1024 (1024) x  480 |        1 | 0x00001b00 | FramebufferSurface                                                                                                          
0xa817de40:  240.00 KiB |  115 ( 128) x  480 |        1 | 0x00000b00 |                                                                                                                             
0xa817e080:  240.00 KiB |  115 ( 128) x  480 |        1 | 0x00000b00 |                                                                                                                             
0xa817f040:  855.00 KiB |  909 ( 912) x  480 |        4 | 0x00000b00 | SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity                                                   
0xa817f100:  240.00 KiB |  115 ( 128) x  480 |        1 | 0x00000b00 |                                                                                                                             
0xa817f340:  855.00 KiB |  909 ( 912) x  480 |        4 | 0x00000b00 | SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity                                                   
0xa817f580: 1920.00 KiB | 1024 (1024) x  480 |        1 | 0x00000b00 | com.adayo.navigationbar/com.adayo.navigationbar.LuancherActivity                                                            
0xa817f940: 1920.00 KiB | 1024 (1024) x  480 |        1 | 0x00000b00 | com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity                                                                 
0xa817fb80: 1920.00 KiB | 1024 (1024) x  480 |        1 | 0x00000b00 | com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity                                                                 
0xa817fd00:  855.00 KiB |  909 ( 912) x  480 |        4 | 0x00000b00 | SurfaceView - com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity                                                   
0xb1c04080:    4.00 KiB | 1024 (1024) x    1 |        1 | 0x00000b00 | StatusBar                                                                                                                   
0xb1c04140:    4.00 KiB | 1024 (1024) x    1 |        1 | 0x00000b00 | StatusBar                                                                                                                   
0xb1c04380: 1920.00 KiB | 1024 (1024) x  480 |        1 | 0x00000b00 | com.autonavi.amapauto/com.autonavi.amapauto.MainMapActivity                                                                 
0xb1c04500:    4.00 KiB | 1024 (1024) x    1 |        1 | 0x00000b00 | StatusBar                                                                                                                   
0xb1c045c0: 4992.00 KiB | 1243 (1248) x 1024 |        2 | 0x00000b00 | com.android.systemui.ImageWallpaper                                                                                         
0xb1fc3a80: 1920.00 KiB | 1024 (1024) x  480 |        1 | 0x00001b00 | FramebufferSurface                                                                                                          
0xb1fc3c00: 1920.00 KiB | 1024 (1024) x  480 |        1 | 0x00001b00 | FramebufferSurface                                                                                                          
Total allocated (estimate): 21729.00 KB                                

Labels (1)
0 Kudos
Reply
5 Replies

4,301 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please tell me which Android version are you using and if you are using our Sabresd board?

Best Regards,

Diego.

0 Kudos
Reply

4,301 Views
giszxl
Contributor I

Hello, the Android version is 7.1.1 with Sabresd board.

0 Kudos
Reply

4,301 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Is there a possibility that you can upgrade to our newer Android version (7.1.2)?

Some errors were fixed in that version, probably the error that you are facing was fixed.

Best regards,

Diego.

0 Kudos
Reply

4,301 Views
giszxl
Contributor I

Hello,

Thanks for your reply. I can not upgrade to Android 7.1.1.  Can you tell me what is the root cause? Is it a mistake about surfaceflinger or a mistake in the hwcomposer hardware device?

Best regards.

0 Kudos
Reply

4,301 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Let me see if I can reproduce your error. However, can you please tell me if you are using our demo image, or is an Android image made by yourself using our BSP.

Best Regards,

Diego.

0 Kudos
Reply