which PMIC is suitable for LPDDR2 with i.MX6Q processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

which PMIC is suitable for LPDDR2 with i.MX6Q processor

3,442 Views
nagaraju_gaddam
Contributor I

Hi,

Iam using i.MX6Q processor and LPDDR2 is interfaced to i.MX6Q processor.

i want now which PMIC is best suitable for this processor with LPDDR2 interface.

thanks

nagaraju gaddam

Labels (2)
0 Kudos
Reply
5 Replies

2,847 Views
YixingKong
Senior Contributor IV

Naga

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos
Reply

2,847 Views
YixingKong
Senior Contributor IV

Naga

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 Kudos
Reply

2,847 Views
SergioSolis
NXP Employee
NXP Employee

For more information you can check the datasheet, page 4

http://cache.freescale.com/files/analog/doc/data_sheet/MMPF0100.pdf


Best regards,
Sergio

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,847 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Nagaraju,

Yes, F1 version is suitable for LPDDR2. As a recommendation and if it is suitable for your application, you can supply 1.2V with SW3 and 1.8V with SW4.

Best regards.

Jorge.

0 Kudos
Reply

2,847 Views
raymondwang
Senior Contributor I

FSL PMIC PF0100F1 should be suitable, right?

0 Kudos
Reply