where to get kobs-ng

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

where to get kobs-ng

3,041件の閲覧回数
bdp42
Contributor IV

Hi,

We are running Android ((iMX Android R10.2 release) on an iMX53 based platform. The host platform is Ubuntu 12.04 LTS. I am looking for the kobs-ng tool to program NAND flash to allow the board boot from NAND and the tool does not seem to be part of the Freescale Android package we are using. It appears to be part of LTIB but from what I can see LTIB is problematic on Ubuntu. e.g. http://www.element14.com/community/thread/23954/l/using-freescales-sources-to-build-an-ltib-image-fo...

I thought I had found the iMX53 executable here https://community.freescale.com/thread/304760 but this did not work when executed on the target. It is possible to get source code from a number of places e.g.  repository.timesys.com/buildsources/k/kobs-ng/http:/ or https://starterkit-org.googlecode.com/files/kobs-ng-11.09.01.tar.gz but is this the right thing to do?

The basic question is what is the best version of kobs-ng for the iMX53 and where can I get it? I don't really want to go through LTIB pain on Ubuntu just to get this one package. Is there an easier way?

Thanks,
Bruno

ラベル(3)
タグ(3)
0 件の賞賛
返信
4 返答(返信)

1,614件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

The kobs-ng was included in the iMX53 Linux BSP. You can get it from the last official released BSP:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX535&nodeId=018rH3ZrDR988D&fpsp=1&...

L2.6.35_11_09_ER_SOURCE

0 件の賞賛
返信

1,614件の閲覧回数
bdp42
Contributor IV

Do I need to use LTIB to build it? The concern I have is that I have seen a number of posts indicating LTIB is problematic on Ubuntu 12.04 and I don't want to get into a new set of pain just to get for this one utility.

Bruno

0 件の賞賛
返信

1,614件の閲覧回数
qiang_li-mpu_se
NXP Employee
NXP Employee

Since you want to use kobs-ng in Android, you should use the Android tool chain to build it, I think you need create an Android.mk for kobs-ng for Android tool chain building.

0 件の賞賛
返信

1,614件の閲覧回数
bdp42
Contributor IV

I guess I was hoping this had been already done by someone and that they would share this out instead of having to reinvent the wheel.

0 件の賞賛
返信