when power on the i.MX6q SABRE Board,The Uboot boot failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

when power on the i.MX6q SABRE Board,The Uboot boot failure

1,336 Views
yangjiao
Contributor I

Hi,

I'll do it strictly according to your tutorials(I.MX6Q ASBRE Board for Smart Devices),I met a problem when power on the i.MX6q SABRE Board,The Uboot boot failure, according to the following:

U-Boot 2016.03-dirty (Aug 05 2016 - 11:06:26 +0800)

CPU: Freescale i.MX6Q rev1.2 996 MHz (running at 792 MHz)

CPU: Automotive temperature grade (-40C to 125C) at 29C

Reset cause: POR

Board: MX6-SabreSD

I2C: ready

DRAM: 1 GiB

force_idle_bus: sda=0 scl=0 sda.gp=0x6d scl.gp=0x6c

force_idle_bus: failed to clear bus, sda=0 scl=0

wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020

i2c_init_transfer: failed for chip 0x8 retry=0

wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020

i2c_init_transfer: failed for chip 0x8 retry=1

wait_for_sr_state: Arbitration lost sr=93 cr=80 state=2020

i2c_init_transfer: failed for chip 0x8 retry=2

i2c_init_transfer: give up i2c_regs=0x21a4000

Can't find PMIC:PFUZE100

initcall sequence 4ff963e4 failed at call 178035f4 (err=-19)

### ERROR ### Please RESET the board ###

Labels (2)
0 Kudos
Reply
2 Replies

763 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Yang Jiao,

It seems that there are problems when u-boot tries to reach the PMIC. It seems that you are using U-Boot 2016.03-dirty. Which BSP are you using with the board? I would recommend trying with the BSP Releases U-Boot versions. For example the U-Boot version from the L4.1.15 release is v2015.04.

Regards,

0 Kudos
Reply

763 Views
yangjiao
Contributor I

Thank you very much,I follow the net link :

https://eewiki.net/display/linuxonarm/i.MX6qSABREBoardforSmart+Devices

Don't show any error or mistake when compile.

I will try use other uboot version.

0 Kudos
Reply