what is the best ARM selection in space applications?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what is the best ARM selection in space applications?

1,608 次查看
vahidnoori
Contributor II

I am seeking a suitable processor for space application among ARM processor in range frequency 500MHz to 800MHz. but I could not find it in freescale products. can you help me?

标记 (3)
0 项奖励
回复
3 回复数

1,377 次查看
LeonardoSandova
Specialist I

what type of user-space applications are you going to develop?

Take a loot at these

i.MX 6 Series Processors

Leo

0 项奖励
回复

1,377 次查看
vahidnoori
Contributor II

i am seeking ARM for startracker in space. which one of imx.6 is suitable for startracker?

0 项奖励
回复

1,377 次查看
Yuri
NXP Employee
NXP Employee

If You mean space / cosmic application special protection features such as memory with ECC should be applied.

Our i.MX series is not intended for such applications. You may take a look at the Layerscape (ARM based).

Layerscape Architecture

Note, it is not launched yet.

0 项奖励
回复