what is default pll values for i.mx6 Soc

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what is default pll values for i.mx6 Soc

1,257 次查看
saida
Contributor II

Hi i.mx6 Community

1. we have brought i.mx6  samples from Freescale part no is MCIMX6D6AVM08 which default frequency is 792Mhz

2. we purchased from vendors some Soc's, part no is MCIMX6D1AVM08 which default frequency is 396Mhz

how to configure it default to 792Mhz ? except writing to  CCM PLL registers

thank you in advance

regards saida

标签 (1)
0 项奖励
回复
3 回复数

1,099 次查看
b36401
NXP Employee
NXP Employee

Actually it is not i.MX6D processor but i.MX6DL one.

As you see its Part Number begins from MCIMX6U not MCIMX6D. 

Here is the description of MCIMX6U1AVM08 signs:

MCIMX6U -- i.MX6DL

1 -- Automotive with MLB and without EPDC, VPU and GPU

A -- Temperature : -40 to + 125C

VM -- MAPBGA 21x21 0.8mm

08 -- 800 (792) MHz

Please note that i.MX 6 Dual and DualLite processors are not the same.

You can refer i.MX 6Solo/6DualLite Applications Processor Reference Manual for the details.

Have a great day,                                                                                                                                                                  

Victor                                                                                                                                                                             

-----------------------------------------------------------------------------------------------------------------------                                                           

Note: If this post answers your question, please click the Correct Answer button. Thank you!                                                                                       

-----------------------------------------------------------------------------------------------------------------------                                                            

0 项奖励
回复

1,099 次查看
b36401
NXP Employee
NXP Employee

I am confused with "1" after "MCIMX6D" in the Part Number.

Officially we have only these options:

4 -- Automotive, with GPU, without VPU 

5 -- Consumer, with VPU and GPU

6 -- Automotive, with VPU and GPU

7 -- Industrial, with VPU and GPU, without MLB

Please make a clear picture of the chip with the Part Number

for I forward it to clarify which processor it is.

Have a great day,

Victor

0 项奖励
回复

1,099 次查看
saida
Contributor II

Hi

Thank your reply my chip part number is MCIMX6U1AVM08

i attaching picture of it please verify and giveme reply

thanks

regards saidaIMG_20160523_144741[1].jpg

0 项奖励
回复