weston

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

weston

1,407件の閲覧回数
gopal_rhsharma
Contributor I

Hi,

I,m using

imx93evk-11x11

DISTRO=fsl-imx-xwayland MACHINE=imx93evk source imx-setup-release.sh -b build-xwayland

BSP 6.6.3

weston 12.0.3

facing problem to load wayland-backend.so

commands like

LayerManagerControl etc. not available please kindly help or suggest to resolving issue.

 

Thanks

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,388件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

You are playing with non-suppoted version and the galcore is passing as module you might try the 6.6.36 bsp.

Regards

0 件の賞賛
返信

1,380件の閲覧回数
gopal_rhsharma
Contributor I
Hi,
our development is going on with BSP 6.6.3. any other method to resolve the problem Rather then to change the BSP.
thanks,
0 件の賞賛
返信