vpu_suspend failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

vpu_suspend failure

1,790 次查看
susangracerapak
Fresh Out Contributor

Hi all,

I am testing suspend and resume functionality on imx6Q with android nougat. When i try suspending, module trying to go into suspend state and getting below issue and then resuming.

dpm_run_callback(): vpu_suspend+0x0/0x158 returns -11
PM: Device 2040000.vpu_fsl failed to suspend: error -11

This is happening continuously (meaning trying to go into suspend and resuming on failure) until i try resume (By moving mouse or pressing power button).

Please help in finding why suspend failing. 

Please find attachment for full log.

Thanks

Susan

0 项奖励
回复
1 回复

1,684 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Susan

one can try to reproduce issue on i.MX6Q Sabre SD reference board with Demo Images from

https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6ser...

If issue can not be reproduced, one can retest ddr memory on custom board and update image

with new memory calibration coefficients found from ddr test:

i.MX6/7 DDR Stress Test Tool V3.00 

Rebuild image from scratch using nxp android sources:

Source Code

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复