video clock timings during kernel logo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

video clock timings during kernel logo

1,325 Views
bblock72
Contributor I

I use an LCD with a pixel clock of 33MHz.  I set my source to pll5 in clk-imx6q.c to allow a clock lower than 38MHz.

I also display a logo from the kernel.

However, during the logo display, the pixel clock measure approx. 8MHz.

After the kernel boots, the pixel clock is 33MHz as desired.

How can I correct the initial pixel clock?

I am using an iMX6q, Linux 3.10.

Labels (3)
0 Kudos
Reply
1 Reply

1,263 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dave

please look at patches provided on

Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply