v4l2_int_device entry is not there when issuing lsmod command (mipi csi2)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

v4l2_int_device entry is not there when issuing lsmod command (mipi csi2)

1,431件の閲覧回数
srinivasaporam
Contributor II

Hi,

We have got IMX6D custom designed board designed based on imx6Q reference board (Wandboard). in custom board we have 512 MB LPDDR2  where as reference board has 1GB/2GB DDR3 RAM.

Now we have connected mipi csi2 camera (Raspi camera (connector is also customized with 15 pin connector)).

When I am running the command for capturing image or video using avconv or gst-launch-1.0 then, image is not being captured.

When iam running the command as :

$ sudo avconv -f video4linux2 -r 30 -s 640x480 -i /dev/video0 out.avi (or)

$ sudo avconv -f video4linux2 -s 640x480 -i /dev/video0 -ss 0:0:2 -frames 1 test.jpg

then it is giving error as ioctl VIDIOC_REQBUFs

and "/dev/video0: No buffer space available"

When we are running this command, we are getting CSI_D0M,CSI_D0P, CSI_D1M, CSI_D1P correctly and laos getting 25 MHz clock from the crystal.

But we are not observing CSI_CLK0M (CN), CSI_CLK0P (CP) are not coming???? what could be the reason.

    $gst-launch-1.0 v4l2src device="/dev/video0" num-buffers=1 ! video/x-bayer,width=640,height=480,framerate=1/1 ! bayer2rgb ! videoconvert ! jpegenc ! filesink location=sample_640_480.jpeg

then it is forming sample_640_480.jpeg file but it is not opening.

in all the above commands, when we are entering/running then led on the camera board is glowing and not when terminating the command, then led is going off.

Following are the findings:

1. camera sensor is being detecting in i2c by using i2c-tools (i2cdetect)

root@ubuntu:~# i2cdetect -y 2

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f

00:          -- -- -- -- -- -- -- -- -- -- -- -- --

10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

30: -- -- -- -- -- -- UU -- -- -- -- -- -- -- -- --

40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --

70: -- -- -- -- -- -- -- --  

2.

root@ubuntu:~# lsmod

Module                  Size  Used by

mxc_v4l2_capture       28532  1

ipu_bg_overlay_sdc      5401  1 mxc_v4l2_capture

ipu_still               2528  1 mxc_v4l2_capture

ipu_prp_enc             5943  1 mxc_v4l2_capture

ipu_csi_enc             3863  1 mxc_v4l2_capture

ipu_fg_overlay_sdc      6217  1 mxc_v4l2_capture

ov5647_camera_mipi     30906  0

Here v4l2_int_device entry is not there.... why v4l2_int_device entry is not there. what could be the problem?????? i have v4l2_int_device.c file and v4l2_int_device.h files. What could be possible error

when iam dumping mipi csi2 regs by using devmem2 tool

[root@erez]# devmem 0x21dc000

0x3130302A

[root@erez]# devmem 0x21dc004

0x1

[root@erez]# devmem 0x21dc008

0x1

[root@erez]# devmem 0x21dc00c

0x1

[root@erez]# devmem 0x21dc010

0x1

[root@erez]# devmem 0x21dc014

0x200

[root@erez]# devmem 0x21dc018

0x0

[root@erez]# devmem 0x21dc020

0x00000000

[root@erez]# devmem 0x21dc024

0x0

[root@erez]# devmem 0x21dc02c

0x00000000

[root@erez]# devmem 0x21dc030

0x0

[root@erez]# devmem 0x21dc034

0x0

These are  dts file entries for reference (wrt mipi csi2)

v4l2_cap_0 {

        compatible = "fsl,imx6q-v4l2-capture";

        ipu_id = <0>;

        csi_id = <1>;

                //csi_id = <0>;

        mclk_source = <0>;

                mipi_camera = <1>;

                default_input = <1>;

        status = "okay";

    };

    v4l2_out {

        compatible = "fsl,mxc_v4l2_output";

        status = "okay";

    };

&i2c3 {

        clock-frequency = <100000>;

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_i2c3_3>;

        status = "okay";

       

       ov5647_mipi@36 {

        compatible = "ovti,ov5647_mipi";

        reg = <0x36>;

        // Pi camera has its own 25MHz clock.

        clocks = <&clks 0>;

        clock-names = "csi_mclk";

       

        DOVDD-supply = <&reg_3p3v>;

        AVDD-supply = <&reg_3p3v>;

        DVDD-supply = <&reg_3p3v>;

        pwn-gpios = <&gpio5 31 GPIO_ACTIVE_HIGH>;

        led-gpios = <&gpio5 19 GPIO_ACTIVE_HIGH>;

        ipu_id = <0>;

        csi_id = <1>;

                //csi_id = <0>;

       

       mclk = <25000000>;

        mclk_source = <0>;

        //pinctrl-names = "default";

        //pinctrl-0 = <&pinctrl_mipi_csi_1>;

         extended-buffer;

          

      };

       

};

&iomuxc {

    pinctrl-names = "default";

    pinctrl-0 = <&pinctrl_hog_1>;

    imx6qdl-wandboard {

        pinctrl_hog_1: hoggrp-1 {

            fsl,pins = <

                             

                                MX6QDL_PAD_CSI0_DAT12__GPIO5_IO30            0x80000000

                                 MX6QDL_PAD_CSI0_DAT13__GPIO5_IO31            0x0f0b0

                                MX6QDL_PAD_CSI0_MCLK__GPIO5_IO19                0x80000000

              >;

};

};

};

&mipi_csi {

    ipu_id = <0>;

    csi_id = <1>;

        //csi_id = <0>;

    v_channel = <0>;

    lanes = <2>;

        mipi_dphy_clk = <0x28>;

    status = "okay";

};

How resolve the issues????

ラベル(4)
0 件の賞賛
返信
1 返信

1,268件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Srinivasa

seems v4l2_int_device is loaded at run time, so if some errors

happen it will not load. You can add debug printfs to trace where

problem occurs.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信