using TV decoder(tvp5158) on IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using TV decoder(tvp5158) on IMX6

ソリューションへジャンプ
19,022件の閲覧回数
hyunhoshin
Contributor III

I'm using tv decoder(tvp5158) on IMX6 and output of tv decoder is BT656(NTSC input,720*480@30fps)

when capture frame using v4l2 application

picture is same as attached files
(frame1~5.jpg)

has anyone idea about this situations?


I'm using Linux 3.0.15 and setting value of csi_param as below

data_width: 1
clk_mode : 2
ext_vsync : 0
Vsync_pol : 0
Hsync_pol : 0
pixclk_pol : 1
data_pol : 0
sens_clksrc : 0
pack_tight : 0
force_eof : 0
data_en_pol : 0
data_fmt : UYVY
csi : 0
mclk : 0

please help me...

ラベル(2)
0 件の賞賛
返信
1 解決策
16,910件の閲覧回数
hyunhoshin
Contributor III

TVP5158 setting was fine

CSI input size was 720 x 525 in base source(IMX6 original code)

I changed that 720 x 525 to 720 x 488 and EAV/SAV code exchange. so, it work fine(no image rolling)

thanks to your opinion.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
16,910件の閲覧回数
翔李
Contributor IV

Hi

I am using tvp5158 on Imx6q board, Linux,can you share your tvp5158 driver source?

My email:[email protected]

thanks.

0 件の賞賛
返信
16,910件の閲覧回数
zhangjay
Contributor II

Hi

I am using tvp5158 on mx53 board, can you share your tvp5158 driver source?

Thanks!

0 件の賞賛
返信
16,910件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,hyunho,

      It seems that image on screen is scrolling up and down , Right ?

Regards,

Weidong

16,910件の閲覧回数
hyunhoshin
Contributor III

you're right, screen is rolling to upside. maybe about 2 pixels every frame

0 件の賞賛
返信
16,910件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,hyunho,

     I judge the issue looks like different CVBS standard. For example:

(1)NTSC

if CVBS camera is NTSC , TVP5158 should be set NTSC standard.

(2)PAL

if CVBS camera is PAL, TVP5158 should be set PAL standard.

So, I feel standard setting in TVP5158 is differenct from it's CVBS signal(camera) input.

check it and try !

Regards,

Weidong

0 件の賞賛
返信
16,910件の閲覧回数
翔李
Contributor IV

Hi

I am using tvp5158 on Imx6q board, Linux,can you share your tvp5158 driver source?

My email:[email protected]

thanks.

0 件の賞賛
返信
16,910件の閲覧回数
zhangjay
Contributor II

Hi

Can you help me with this issue?

https://community.freescale.com/message/358505#358505

0 件の賞賛
返信
16,911件の閲覧回数
hyunhoshin
Contributor III

TVP5158 setting was fine

CSI input size was 720 x 525 in base source(IMX6 original code)

I changed that 720 x 525 to 720 x 488 and EAV/SAV code exchange. so, it work fine(no image rolling)

thanks to your opinion.

0 件の賞賛
返信
16,910件の閲覧回数
翔李
Contributor IV

Hi

I am using tvp5158 on Imx6q board, Linux,can you share your tvp5158 driver source?

My email:[email protected]

0 件の賞賛
返信