usb upgrade

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb upgrade

1,423 Views
yufe
Contributor II

two imx6d board connetc with usb, one run android and the other run linux. i want upgrade linux board through usb, is there a proper way to do this?

Labels (1)
0 Kudos
Reply
2 Replies

1,311 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

You can use the mfgtool nxp provide to download the new linux images to your board. Via the usb-otg line connect your board to PC to download.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,311 Views
yufe
Contributor II

my hardware is not support this mode, boot conf pins are fixed. host android board and salve linux borad connect through usb only.

is there a way to upgrade uboot, kernel or fs? i see tplink route and other product support internet online upgrade, can usb do the same thing?

0 Kudos
Reply