usb porting in uboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usb porting in uboot

1,183 Views
lixuhui112
Contributor I

hello all:

my board base on imx6qsabreauto ,in my board usb .png

and how can  Configuration it  in my code

Thank you!

Labels (1)
0 Kudos
Reply
1 Reply

1,093 Views
igorpadykov
NXP Employee
NXP Employee

Hi xuhi

usb is supported in uboot, please check

http://git.freescale.com/git/cgit.cgi/imx/uboot-imx.git/tree/?h=imx_v2015.04_4.1.15_1.0.0_ga

one can just verify that 5V (V5USB) was provided on USB connector.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply