usage eMMC in pSLC mode with imx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

usage eMMC in pSLC mode with imx6

Jump to solution
4,326 Views
jindrichbrett
Contributor II

Hi imx linux guys,

I would like to ask if anybody uses eMMC in pSLC mode with imx6. I personally have no experiences with that, but my quite experienced customer told me that there is still no support for that mode in linux kernel for imx6 - specific register is not accesible.. 

Second source tels me that this is not imx-specific question. it should work transparently like standard emmc and only tehe is necesarry to "format" ( setup ) card to that mode.

if anybody knows answer please let me know.

Thanks  a lot

Jindrich

Labels (1)
0 Kudos
Reply
1 Solution
3,115 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jindrich

advantage of pSLC is that it does not require any changes to the memory controller

so it is used as usual eMMC:

http://electronicdesign.com/site-files/electronicdesign.com/files/uploads/2013/09/FAQs-Toshiba-Septe...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
3,116 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jindrich

advantage of pSLC is that it does not require any changes to the memory controller

so it is used as usual eMMC:

http://electronicdesign.com/site-files/electronicdesign.com/files/uploads/2013/09/FAQs-Toshiba-Septe...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,116 Views
jindrichbrett
Contributor II

Hi Igor,

ok, thanks a lot.

Jindrich

0 Kudos
Reply
3,116 Views
jindrichbrett
Contributor II

Hi Igor,

Have you got some experiences how to setup pslc mode please ?

is it necesarry to write several register directly to emmc, or does exist some routine for linux ?

what i know so our programming centre is able to do that, but they do not want to share what everything is necesarry.

Thanks

BR

JIndrich

0 Kudos
Reply