unused QSPI pins for i.MX 8QuadXPlus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

unused QSPI pins for i.MX 8QuadXPlus

跳至解决方案
1,858 次查看
Derun93
Contributor II

Hi everyone,

I am designing a single board computer with i.MX 8QuadXPlus. I do not need processor booting up from QSPI. So what should I do related QSPI pins of i.MX 8QuadXPlus? Tie to Gnd or leave floating?

In hardware guide, it says we can leave floating power pins of QSPI bank but nothing about data, clock and strobe pins.

Thank you. 

0 项奖励
回复
1 解答
1,847 次查看
Derun93
Contributor II

Thank you @igorpadykov for your answer. Just to be clear, if I add pull-up resistor, do these pins become input or are they already inputs with internal pull-up?

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,851 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Derun

 

unused qspi pins can be left unconnected,  one can configure them as inputs with pull-up enabled.

 

Best regards
igor

1,848 次查看
Derun93
Contributor II

Thank you @igorpadykov for your answer. Just to be clear, if I add pull-up resistor, do these pins become input or are they already inputs with internal pull-up?

0 项奖励
回复
1,842 次查看
igorpadykov
NXP Employee
NXP Employee
0 项奖励
回复