unused QSPI pins for i.MX 8QuadXPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unused QSPI pins for i.MX 8QuadXPlus

Jump to solution
1,174 Views
Derun93
Contributor II

Hi everyone,

I am designing a single board computer with i.MX 8QuadXPlus. I do not need processor booting up from QSPI. So what should I do related QSPI pins of i.MX 8QuadXPlus? Tie to Gnd or leave floating?

In hardware guide, it says we can leave floating power pins of QSPI bank but nothing about data, clock and strobe pins.

Thank you. 

0 Kudos
Reply
1 Solution
1,163 Views
Derun93
Contributor II

Thank you @igorpadykov for your answer. Just to be clear, if I add pull-up resistor, do these pins become input or are they already inputs with internal pull-up?

View solution in original post

0 Kudos
Reply
3 Replies
1,167 Views
igorpadykov
NXP Employee
NXP Employee

Hi Derun

 

unused qspi pins can be left unconnected,  one can configure them as inputs with pull-up enabled.

 

Best regards
igor

1,164 Views
Derun93
Contributor II

Thank you @igorpadykov for your answer. Just to be clear, if I add pull-up resistor, do these pins become input or are they already inputs with internal pull-up?

0 Kudos
Reply
1,158 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos
Reply