unable to load module vivante

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

unable to load module vivante

1,295 Views
prathameshghane
Contributor II

Hi all,

I am facing this error when try to run startx on imx6 board.

[    36.794] (II) LoadModule:"vivante"                                          

[    36.808] (II) Loading /usr/lib/xorg/modules/input/vivante_drv.so

[   36.920] (EE) LoadModule: Module vivante does not have a vivanteModuleData data object.

[   36.920] (II) UnloadModule:"vivante"                                                

[   36.920] (II) Unloading vivante                                   
[   36.938] (EE) Failed to load module "vivante" (invalid module, 0)                    

[    36.938] (EE) No drivers available.                                       

Can anyone help me in this regard??

Apart from this, can you also explain the standard procedure to bring up the vivante GPU during startup scripts?

Thanks and regards,

Prathamesh

Labels (3)
0 Kudos
Reply
0 Replies