udoo boot from emmc flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

udoo boot from emmc flash

1,848 Views
dillibabug
Contributor I

hi,
we developing project in udoo neo board with android os, we want to boot the android os from emmc flash, i have checked udoo neo board schematic the J4 & J6 have SDIO interface. could you tell us how to boot from emmc flash and also suggest any emmc flash which is suitable for udoo neo.

thank you...

Labels (1)
0 Kudos
Reply
2 Replies

1,710 Views
jealcuna
Contributor I

UDOO NEO does not have eMMC memory, so an OS just can be loaded from SD card.

0 Kudos
Reply

1,710 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Dillibabu,

NXP does not support Udoo board as it is not developed by NXP. You can contact www.udoo.org for support.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply