uboot logo

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot logo

3,561件の閲覧回数
fulinux
Contributor IV

board: imx6q;

version: u-boot-2009.08;

Dear Community,

     i want to show logo on my 1920x1080 lcd panel, it uses lvds split mode in kernel, my kernel can show logo, how can i modify the uboot to show logo, it seems only set one lvds, Are there any examples ?

then, i did as this doc Patch to support uboot logo keep from uboot to kernel for NXP Linux and Android BSP (HDMI, LCD and L... said, and make -j2, it shows some error as following:

board/freescale/mx6q_sabresd/libmx6q_sabresd.a(mx6q_sabresd.o): In function `board_late_init':

/home/fulinux/u-boot-qt/board/freescale/mx6q_sabresd/mx6q_sabresd.c:2078: undefined reference to `ipu_display_setup'

common/libcommon.a(lcd.o): In function `console_newline':

/home/fulinux/u-boot-qt/common/lcd.c:159: undefined reference to `panel_info'

common/libcommon.a(lcd.o): In function `lcd_putc':

/home/fulinux/u-boot-qt/common/lcd.c:200: undefined reference to `panel_info'

common/libcommon.a(lcd.o): In function `lcd_setmem':

/home/fulinux/u-boot-qt/common/lcd.c:476: undefined reference to `panel_info'

common/libcommon.a(lcd.o): In function `lcd_display_bitmap':

/home/fulinux/u-boot-qt/common/lcd.c:829: undefined reference to `panel_info'

common/libcommon.a(lcd.o): In function `lcd_clear':

/home/fulinux/u-boot-qt/common/lcd.c:415: undefined reference to `panel_info'

common/libcommon.a(lcd.o): In function `lcd_init':

/home/fulinux/u-boot-qt/common/lcd.c:433: undefined reference to `lcd_enable'

common/libcommon.a(lcd.o): In function `drv_lcd_init':

/home/fulinux/u-boot-qt/common/lcd.c:369: undefined reference to `panel_info'

drivers/video/libvideo.a(mxc_ipuv3_fb.o): In function `calc_fbsize':

/home/fulinux/u-boot-qt/drivers/video/mxc_ipuv3_fb.c:612: undefined reference to `panel_info'

drivers/video/libvideo.a(mxc_ipuv3_fb.o): In function `lcd_ctrl_init':

/home/fulinux/u-boot-qt/drivers/video/mxc_ipuv3_fb.c:633: undefined reference to `panel_info'

drivers/video/libvideo.a(mxc_ipuv3_fb.o): In function `ipuv3_fb_init':

/home/fulinux/u-boot-qt/drivers/video/mxc_ipuv3_fb.c:649: undefined reference to `panel_info'

drivers/video/libvideo.a(ipu_common.o): In function `clk_ipu_enable':

/home/fulinux/u-boot-qt/drivers/video/ipu_common.c:166: undefined reference to `ipu_clk_enable'

what should i do? should i define panel_info in mx6q_sabresd.c file, and where?

need help!

fulinux.

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,804件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi fulinux

seems you used wrong uboot, please try to build from i.MX6 product page

Board Support Packages (38)

i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo and i.MX 6Sololite Linux

BSP Source Code Files (REV L3.0.35_4.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

or from

Index of /buildsources/u/u-boot/u-boot-2009.08

and use Chapter 1 Porting U-Boot attached Porting Guide.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,803件の閲覧回数
fulinux
Contributor IV

Dear igor,

this picture of lcd screen status, what's wrong?

P60512-160237.jpg

0 件の賞賛
返信

2,803件の閲覧回数
fulinux
Contributor IV

Hi igor,

it is ok when i make distclean && make;

thank you.

fulinux.

0 件の賞賛
返信

2,804件の閲覧回数
fulinux
Contributor IV

and it happend this:

Map u-boot.map -o u-boot

arm-linux-gnueabi-ld: cannot find common/env_embedded.o

make: *** [u-boot] Error 1

0 件の賞賛
返信