uboot fetch-error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

uboot fetch-error

1,689件の閲覧回数
oliver_meier
Contributor I

Hello,

I try to build the adv-arm-yocto-bsp "imx6LBV90019" for the ROM5420b1 module.

During the build process it trys to fetch uboot "imx_v2018.03_4.14.98_2.0.0_ga" and this fails.

I get the following error messages:

WARNING: u-boot-imx-2018.03-r0 do_fetch: Failed to fetch URL git://github.com/ADVANTECH-Corp/uboot-imx6.git;protocol=https;branch=imx_v2018.03_4.14.98_2.0.0_ga;branch=imx_v2018.03_4.14.98_2.0.0_ga, attempting MIRRORS if available


ERROR: u-boot-imx-2018.03-r0 do_fetch: Fetcher failure: Unable to find revision bb7adf20c05448b7cb3088d6d03a17482a44ad5f in branch imx_v2018.03_4.14.98_2.0.0_ga even from upstream
ERROR: u-boot-imx-2018.03-r0 do_fetch: Fetcher failure for URL: 'git://github.com/ADVANTECH-Corp/uboot-imx6.git;protocol=https;branch=imx_v2018.03_4.14.98_2.0.0_ga;branch=imx_v2018.03_4.14.98_2.0.0_ga'. Unable to fetch URL from any source.

ERROR: u-boot-imx-2018.03-r0 do_fetch: Function failed: base_do_fetch
ERROR: Logfile of failure stored in: /home/adv/adv-release-bsp/build/tmp/work/imx6qrom5420b1-poky-linux-gnueabi/u-boot-imx/2018.03-r0/temp/log.do_fetch.77929
ERROR: Task (/home/adv/adv-release-bsp/sources/meta-fsl-bsp-release/imx/meta-bsp/recipes-bsp/u-boot/u-boot-imx_2018.03.bb:do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2771 tasks of which 2737 didn't need to be rerun and 1 failed.

- Is this an Server/GitHub problem or does the build script try to fetch the wrong uboot version?

GitHub - ADVANTECH-Corp/uboot-imx6 at imx_v2018.03_4.14.98_2.0.0_ga  seems to exist, so what can be the problem here?

Build environment:

I use Ubuntu 16.04 (u16.04-imx8lbv1) following this guide:

Yocto Linux BSP Ver.9 User Guide for iMX6 series - ESS-WIKI 

Any Ideas?

Best Regards,

Oliver

0 件の賞賛
返信
1 返信

1,598件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Oliver,

The ROM-5420 B1 is manufactured and supported by Advantech, so they may be able to better assist you.

The branch does exist, and it does not seem like it’s a connectivity issue. It looks like it’s giving the branch information twice, maybe that’s part of the problem.

'git://github.com/ADVANTECH-Corp/uboot-imx6.git;protocol=https;branch=imx_v2018.03_4.14.98_2.0.0_ga;branch=imx_v2018.03_4.14.98_2.0.0_ga'.

Regards,

0 件の賞賛
返信