uBoot iMX6 Quad versus Dual (differentiation)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uBoot iMX6 Quad versus Dual (differentiation)

Jump to solution
1,126 Views
juliocruz
Contributor III

Hi All,

I have two boards:

  1. QUAD with 2GB DDR3
  2. DUAL with 1GB DDR3

I would like to create a unified u-boot that could setup/config the RAM in SPL stage.

My question is: there is a way to know if the board have a QUAD or DUAL?

The function "get_cpu_rev" does not help too much. Additionally, the current header definitions seems no have the dual:

#define MXC_CPU_MX510x51
#define MXC_CPU_MX530x53
#define MXC_CPU_MX6SL0x60
#define MXC_CPU_MX6DL0x61
#define MXC_CPU_MX6SOLO0x62
#define MXC_CPU_MX6Q0x63

Thanks

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
947 Views
igorpadykov
NXP Employee
NXP Employee

Hi Julio

i.MX6 Quad versus Dual differentiated by fuse NUM_CORES (0x430) 

Table 5-10 Fusemap Descriptions  IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
948 Views
igorpadykov
NXP Employee
NXP Employee

Hi Julio

i.MX6 Quad versus Dual differentiated by fuse NUM_CORES (0x430) 

Table 5-10 Fusemap Descriptions  IMX6DQRM

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
947 Views
juliocruz
Contributor III

Hi Igor,

Thanks for your reply!

Julio

0 Kudos
Reply