I'm trying to understand how uBoot knows where to find the necessary hardware and peripherals on the IMX6. For example, when I build the default image uBoot outputs over UART1, but is it possible to have default output on UART2, 3,.. etc. Is there something similar to the DTB that uBoot uses to know what hardware it has available?
解決済! 解決策の投稿を見る。
Hi danielbujak
there is no dtb in uboot, typically some modifications can be set in
uboot/include/configs/board_name.h file. Other hardware changes are
manually entered in code, please also look at attached Porting Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I found the changes required for the UART:
mx6ul_14x14_evk.h:
#define CONFIG_MXC_UART_BASE UART2_BASE
and
mx6ul_14x14_evk.c:
static iomux_v3_cfg_t const uart2_pads[] = {
MX6_PAD_NAND_DATA04__UART2_DCE_TX | MUX_PAD_CTRL(UART_PAD_CTRL),
MX6_PAD_NAND_DATA05__UART2_DCE_RX | MUX_PAD_CTRL(UART_PAD_CTRL),
};
Hi danielbujak
there is no dtb in uboot, typically some modifications can be set in
uboot/include/configs/board_name.h file. Other hardware changes are
manually entered in code, please also look at attached Porting Guide.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------