Hi all,
I'm using tv decoder(tvp5158) on imx27, using the 4 channel half D1 mode.
I config the register by using i2c, and set the interface param as below:
param->Vsync_pol = 0x0; | ||
param->clk_mode = 0x0; | //gated | |
param->pixclk_pol = 0x0; | ||
param->data_width = 0x1; | ||
param->data_pol = 0x0; | ||
param->ext_vsync = 0x1; | ||
param->Vsync_pol = 0x0; | ||
param->Hsync_pol = 0x0; | ||
param->width = width - 1; | ||
param->height = height - 1; | ||
param->pixel_fmt = IPU_PIX_FMT_UYVY; | ||
param->mclk = 54000000; | ||
/* setup cropping */ |
when insert the mode, I use the mxc_v4l2_capture test tool to capture image, but I always get the error log
mx27# ./mxc_v4l2_capture.out -w 360 -h 480 -c 1 /mnt/sample.yuv
g_width = 360, g_height = 480
TVP5158 Chip version = TVP5158
====>chip id: tvp5158
Patch is downloading...
0xa2 0x10 0x25 0xe5 0xe8 0x00 0x1b 0x04
0x1e 0x90 0xa5 0x00 0x02 0x01 0x14 0x00 0x51 0x58 0x0d 0x02 0x81 0x00 0x03 0x03
0x80 0x80 0x00 0x80 0x00 0x00 0x10 0x0a 0x40 0x00 0x00 0x00 0x0c 0x00 0x00 0x00
0x00 0x00 0x00 0x80 0x00 0xf5 0x00 0x00 0x00 0x06 0x1e 0x04 0x00 0xf2 0x08 0x04
0xff 0xff 0x00 0x00 0x6a 0x08 0x05 0x07 0x7a 0x00 0xd0 0x02 0x19 0x00 0xf0 0x00
0x25 0x03 0x40 0x00 0x04 0x00 0x07 0x00 0x7a 0x00 0xd0 0x02 0x01 0x00 0x15 0x00
0x7a 0x00 0xd0 0x02 0x8d 0x00 0xbc 0x02 0x26 0x00 0xdc 0x00 0x1e 0x09 0x34 0x03
0x00 0x09 0x40 0x1e 0x18 0x00 0x0b 0x00 0x00 0x1f 0x1f 0x02 0x10 0x04 0x64 0x20
0x7d 0x00 0x8a 0x64 0x04 0x02 0x0f 0x0f 0x03 0x05 0x20 0x1e 0x02 0x08 0x03 0x03
0x0a 0x00 0x5a 0x06 0x00 0x03 0x22 0x00 0x00 0x16 0x1d 0x64 0x00 0x00 0x0a 0x04
0x10 0x80 0x80 0x00 0x00 0x00 0x60 0x50 0x00 0x00 0x00 0x0a 0x05 0x05 0x03 0xbc
0xbc 0x00 0x0d 0x02 0x90 0x01 0x78 0x00 0x44 0x40 0x03 0xd8 0x05 0x00 0x01 0x00
0xa2 0x10 0x25 0xe5 0xe8 0x00 0x1b 0x04 0x40 0x00 0x00 0x01 0xd7 0x0f 0x00 0x00
0x00 0x88 0x88 0xe0 0x01 0x00 0x00 0x00 0x00 0xa5 0xff 0x7e 0x01 0x00 0x00 0x00
0x70 0x00 0xd8 0x02 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
0x02 0x02 0x00 0x00 0x25 0x25 0x25 0x25 0x61 0x00 0xb0 0x00 0x00 0x00 0x02 0x25
0x08 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x25 0x25 0x25 0x25 0x25 0x0f ====>chip id: tvp5158
Patch is already running
0xa2 0x10 0x25 0xe5 0xe8 0x00 0x1b 0x04
0x1e 0x90 0xa6 0x00 0x02 0x01 0x14 0x00 0x51 0x58 0x0d 0x02 0x81 0x00 0x03 0x03
0x80 0x80 0x00 0x80 0x00 0x00 0x10 0x0a 0x40 0x00 0x00 0x00 0x0c 0x00 0x00 0x00
0x00 0x00 0x00 0x80 0x00 0xf5 0x00 0x00 0x00 0x06 0x1e 0x04 0x00 0xf2 0x08 0x04
0xff 0xff 0x00 0x00 0x6a 0x08 0x05 0x07 0x7a 0x00 0xd0 0x02 0x19 0x00 0xf0 0x00
0x25 0x03 0x40 0x00 0x04 0x00 0x07 0x00 0x7a 0x00 0xd0 0x02 0x01 0x00 0x15 0x00
0x7a 0x00 0xd0 0x02 0x8d 0x00 0xbc 0x02 0x26 0x00 0xdc 0x00 0x1e 0x09 0x34 0x03
0x00 0x09 0x40 0x1e 0x18 0x00 0x0b 0x00 0x00 0x1f 0x1f 0x02 0x10 0x04 0x64 0x20
0x7d 0x00 0x8a 0x64 0x04 0x02 0x0f 0x0f 0x03 0x05 0x20 0x1e 0x02 0x08 0x03 0x03
0x0a 0x00 0x5a 0x06 0x00 0x03 0x22 0x00 0x00 0x16 0x1d 0x64 0x00 0x00 0x0a 0x04
0x10 0x80 0x80 0x00 0x00 0x00 0x60 0x50 0x00 0x00 0x00 0x0a 0x05 0x05 0x03 0xbc
0xbc 0x00 0x0d 0x02 0x90 0x01 0x78 0x00 0x44 0x40 0x03 0xd8 0x05 0x00 0x01 0x00
0xa2 0x10 0x25 0xe5 0xe8 0x00 0x1b 0x04 0x40 0x00 0x00 0x01 0xd7 0x0f 0x00 0x00
0x00 0x88 0x88 0xe0 0x01 0x00 0x00 0x00 0x00 0xa5 0xff 0x7e 0x01 0x00 0x00 0x00
0x70 0x00 0xd8 0x02 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00
0x02 0x02 0x00 0x00 0x25 0x25 0x25 0x25 0x61 0x00 0xb0 0x00 0x00 0x00 0x02 0x25
0x08 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x25 0x25 0x25 0x25 0x25 0x0f Width = 360 Height = 480 Image size = 259200
pixelformat = 842093913
<3>mxc_v4l_dqueue timeout enc_counter 0
VIDIOC_DQBUF failed.
buf.index 0
mx27#
Attachment file is my tvp5158 driver, anyone can give me some advice?
Please help me.
Original Attachment has been moved to: tvp5158.c.txt.zip
已解决! 转到解答。
I am not sure how tvp5158 and tvp5150 are similar, but I would suggest you to take a look at the latest kernel that has support for the mx25 visstrim board, which is connected to a tvp5150:
The tvp5150 driver is located at:
Hope this helps.
Regards,
Fabio Estevam
I am not sure how tvp5158 and tvp5150 are similar, but I would suggest you to take a look at the latest kernel that has support for the mx25 visstrim board, which is connected to a tvp5150:
The tvp5150 driver is located at:
Hope this helps.
Regards,
Fabio Estevam