While playing video by gplayer on Yocto 1.8, the position of video window is not started at [0,0] on the monitor
I used the command:
gplay-1.0 mpeg2sample.mpg --video-sink="imxv4l2sink overlay-width=600 overlay-height=480"
Are there any advice about the issue?
Thanks
Solved! Go to Solution.
try to use overlaysink to replace the imxv4l2sink, and try to use the parameter
overlay-top : The topmost (y) coordinate of the video overlay; top left corner of screen is 0...
try to use overlaysink to replace the imxv4l2sink, and try to use the parameter
overlay-top : The topmost (y) coordinate of the video overlay; top left corner of screen is 0...
Hi Guanqiong Xie,
I play this command on Yocto 1.8
gst-launch-1.0 playbin uri=file:///run/media/sda/wetransfer-fd47c1/mpeg2sample.mpg video-sink="imxvideoconvert_ipu rotation=0 ! overlaysink overlay-top=0 overlay-left=0 overlay-width=640 overlay-height=480 display=:0"
The result is
Black zone is full screen and video is still not started at [0,0] , one video is maybe at [0, 10] and another one is at [5, 0].
and are there any solutions to play video on windows mode of black zone, not full screen ?