transplant kernel to imx6ul

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

transplant kernel to imx6ul

1,085 次查看
victorsong
Contributor I

I tried to transplant kernel-4.14.6 to imx6ul.but always bug and error here and there.

now,when u-boot boot the kernel shows that:

[<80118ff4>] (imx_gpc_mask_all) from [<8011a094>] (imx6_enable_rbc+0x14/0x78)
[<8011a094>] (imx6_enable_rbc) from [<80c09090>] (imx6sx_cpuidle_init+0x14/0x40)
[<80c09090>] (imx6sx_cpuidle_init) from [<80c09568>] (imx6ul_init_late+0xc/0x40)
[<80c09568>] (imx6ul_init_late) from [<80c0364c>] (init_machine_late+0x20/0x98)
[<80c0364c>] (init_machine_late) from [<80101990>] (do_one_initcall+0x40/0x16c)
[<80101990>] (do_one_initcall) from [<80c00dc4>] (kernel_init_freeable+0x144/0x1e0)
[<80c00dc4>] (kernel_init_freeable) from [<808757a0>] (kernel_init+0x8/0x110)
[<808757a0>] (kernel_init) from [<80107aa8>] (ret_from_fork+0x14/0x2c)
Code: e5913010 e2812014 e2811024 e2833008 (e5930000)
---[ end trace bb46de54d68d47a3 ]---
Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b

hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
random: crng init done

how could i solve this ?

0 项奖励
回复
0 回复数