test code for checking ECSPI2 on iMX8M Mini EVK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

test code for checking ECSPI2 on iMX8M Mini EVK

ソリューションへジャンプ
2,769件の閲覧回数
sreedhar_appala
Contributor III

Hi,

I am working with IMX8M Mini EVK and yocto project build details:

 

Build Configuration:
BB_VERSION = "1.38.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "ubuntu-16.04"
TARGET_SYS = "aarch64-poky-linux"
MACHINE = "imx8mmevk"
DISTRO = "fsl-imx-xwayland"
DISTRO_VERSION = "4.14-sumo"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""

I have enabled the ECSPI2 in the dts file as mentioned in the thread ECSPI2 on i.MX8M Mini EVK 

Could you please share me any test code to do the ECSPI2 test.

Is this the location of test code : 

imx-yocto-bsp/<yocto-build>/tmp/work/aarch64-mx8mm-poky-linux/imx-test/1_7.0+AUTOINC+d32727a9d7-r0/git/test/mxc_spi_test       

Thank you, Sreedhar

ラベル(3)
0 件の賞賛
返信
1 解決策
2,663件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

one can look at attached patch or example of nitrogen board

linux-imx6/imx8mm-nitrogen8mm.dts at boundary-imx_4.14.x_1.0.0_ga · boundarydevices/linux-imx6 · Git... 

unit tests for test  :

mxc_spi_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,664件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Sreedhar

one can look at attached patch or example of nitrogen board

linux-imx6/imx8mm-nitrogen8mm.dts at boundary-imx_4.14.x_1.0.0_ga · boundarydevices/linux-imx6 · Git... 

unit tests for test  :

mxc_spi_test\test - imx-test - i.MX Driver Test Application Software 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,663件の閲覧回数
sreedhar_appala
Contributor III

Thank you igor,

you gave me the details what i am looking far.

thanks once again,

Sreedhar

0 件の賞賛
返信